EtherNet/IP™ Adapter  2.01.00

◆ EI_API_ADP_getTimeSyncProductDescription()

uint32_t EI_API_ADP_getTimeSyncProductDescription ( T *  pAdp_p,
char *  pProductDesc_p 
)

Get the Description member of the ProductDescription attribute of the Time Sync Object (Instance Attribute ID: 21).

Function that returns the Description member of the ProductDescription attribute of the Time Sync Object for the adapter selected by parameter pAdp_p in output parameter pProductDesc_p.

Parameters
[in]pAdp_pPointer to the adapter.
[out]pProductDesc_pchar pointer to ProductDescription.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
char productDesc[64];
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
errCode = EI_API_ADP_getTimeSyncProductDescription(pEI_API_ADP, pProductDesc_p);
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:301
ETHIP_API uint32_t EI_API_ADP_getTimeSyncProductDescription(T *pAdp_p, char *pProductDesc_p)
Get the Description member of the ProductDescription attribute of the Time Sync Object (Instance Attr...
Definition: EI_API_ADP_main.c:2763
See also
EI_API_ADP_setTimeSyncProductDescription EI_API_ADP_EError_t