EtherNet/IP™ Adapter  2.01.00

◆ EI_API_ADP_setHwConfigurable()

uint32_t EI_API_ADP_setHwConfigurable ( T *  pAdp_p,
bool  bHwConfigurable_p 
)

Sets the capability to set the IP address by hardware.

Let the EtherNet/IP stack know that the IP address is configurable by hardware or not.

Parameters
[in]pAdp_pPointer to the adapter.
[in]bHwConfigurable_pHardware setting not configurable/configurable (0/1).
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
errCode = EI_API_ADP_setHwConfigurable(pEI_API_ADP, true);
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:301
ETHIP_API uint32_t EI_API_ADP_setHwConfigurable(T *pAdp_p, bool hwConfigurable_p)
Sets the capability to set the IP address by hardware.
Definition: EI_API_ADP_main.c:5802
See also
EI_API_ADP_isHwSettingEnabled