EtherNet/IP™ Adapter  2.01.00

◆ EI_API_ADP_setQuickConnectEnabled()

uint32_t EI_API_ADP_setQuickConnectEnabled ( T *  pAdp_p,
bool  quickConnectEnabled_p 
)

Set the current adapter QuickConnect state (Instance Attribute ID: 12).

This function sets the EtherNet/IP Adapter QuickConnect state.

Value Description
0 Disable
1 Enable
Parameters
[in]pAdp_pPointer to the adapter.
[in]quickConnectEnabled_pThe QuickConnect state.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
// Enable QuickConnect
errCode = EI_API_ADP_setQuickConnectEnabled(pEI_API_ADP, 1);
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:301
ETHIP_API uint32_t EI_API_ADP_setQuickConnectEnabled(T *pAdp_p, bool quickConnectEnabled_p)
Set the current adapter QuickConnect state (Instance Attribute ID: 12).
Definition: EI_API_ADP_main.c:5139
See also
EI_API_ADP_getQuickConnectEnabled EI_API_ADP_EError_t