EtherNet/IP™ Adapter  2.01.00

◆ EI_API_ADP_setVendorId()

uint32_t EI_API_ADP_setVendorId ( T *  pAdp_p,
uint16_t  vendorId_p 
)

Set the adapter Vendor ID (Instance Attribute ID: 1).

Function that can be used to set the current adapter vendor identifier to the value assigned by ODVA. The value zero is reserved.

Parameters
[in]pAdp_pPointer to the adapter.
[in]vendorId_pNew vendor identifier.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
// Set vendor ID to Texas Instruments (806)
errCode = EI_API_ADP_setVendorId(pEI_API_ADP, 0x326);
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:301
ETHIP_API uint32_t EI_API_ADP_setVendorId(T *pAdp_p, uint16_t vendorId_p)
Set the adapter Vendor ID (Instance Attribute ID: 1).
Definition: EI_API_ADP_main.c:1059
See also
EI_API_ADP_getVendorId EI_API_ADP_EError_t