#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:301
ETHIP_API uint32_t EI_API_ADP_getIntfConfig(T *pAdp_p, uint8_t intfId_p, EI_API_ADP_UIntfConf_t *pIntfConf_p)
Get the current adapter configuration of interface with the specified ID (Instance Attribute ID: 6).
Definition: EI_API_ADP_main.c:5419
Structure to use as function parameter (attribute parameters)
Definition: EI_API_def.h:213