#include <api/EI_API.h>
void errorHandlerFunc(uint32_t errorCode_p, uint8_t fatal_p, uint8_t numOfParam_p, va_list arg_p);
{
}
void registerStackErrorHandler()
{
uint32_t errCode;
}
ETHIP_API uint32_t EI_API_ADP_setErrorHandlerFunc(EI_API_ADP_CBStackError callback_p)
Set the stack error handler function.
Definition: EI_API_ADP_main.c:827
void(* EI_API_ADP_CBStackError)(uint32_t errorCode_p, uint8_t fatal_p, uint8_t numOfParam_p, va_list arg_p)
Function prototype for general stack error callback.
Definition: EI_API_def.h:332