EtherCAT Slave1.11.00

◆ EC_API_SLV_FoE_cbRegisterOpenFileHandler()

void EC_API_SLV_FoE_cbRegisterOpenFileHandler ( EC_API_SLV_SHandle_t pEcSlaveApi_p,
void *  pContext_p,
EC_API_SLV_FoE_CBOpenFileHandler_t  cbFunc_p 
)

This is the function to register FoE open function.

This function registers a function pointer which must be implemented by the user. The user defined function will be called if a file read or write request is received from the master.

Parameters
[in]pEcSlaveApi_pThe pointer to the EtherCAT API instance.
[in]pContext_popenFileHandler call context
[in]cbFunc_pFunction pointer to the FoE Open file Handler
Example
#include <ecSlvApi.h>
// the Call
EC_API_SLV_FoE_cbRegisterOpenFileHandler(ecSlaveApi, ecSlaveApi, cbFunc);
EC_API_SLV_FoE_cbRegisterOpenFileHandler
void EC_API_SLV_FoE_cbRegisterOpenFileHandler(EC_API_SLV_SHandle_t *pEcSlaveApi_p, void *pContext_p, EC_API_SLV_FoE_CBOpenFileHandler_t cbFunc_p)
This is the function to register FoE open function.
Definition: ecSlvApi_FoEStub.c:82