EtherCAT Slave
1.11.00
◆
EC_API_SLV_getCyclicStatus()
uint32_t EC_API_SLV_getCyclicStatus
(
EC_API_SLV_SHandle_t
*
pEcSlaveApi_p
)
This function reads if there is any error cyclic communication error.
Parameters
[in]
pEcSlaveApi_p
The pointer to the EtherCAT API instance.
Returns
EC_API_EError_t Returns the API error code.
Example
#include <ecSlvApi.h>
EC_API_EError_t
error =
EC_API_SLV_getCyclicStatus
(ecSlaveApi);
EC_API_SLV_getCyclicStatus
uint32_t EC_API_SLV_getCyclicStatus(EC_API_SLV_SHandle_t *pEcSlaveApi_p)
This function reads if there is any error cyclic communication error.
Definition:
ecSlvApiStub.c:891
EC_API_EError_t
enum EC_API_EError EC_API_EError_t
Basic Functions
generated by
1.8.17