AM64x MCU+ SDK  08.05.00
Udma_EventRxFlowIdFwStatus Struct Reference

Detailed Description

UDMAP receive flow id firewall status.

This structure contains status information collected whenever the receive flow ID firewall detects a flow ID that is out of range for an incoming packet.

Data Fields

uint32_t isException
 
uint32_t flowId
 
uint32_t chNum
 

Field Documentation

◆ isException

uint32_t Udma_EventRxFlowIdFwStatus::isException

This is set whenever the Flow ID firewall detects a Flow ID is out of range for an incoming packet.

◆ flowId

uint32_t Udma_EventRxFlowIdFwStatus::flowId

[OUT] The flow ID that was received on the trapped packet

◆ chNum

uint32_t Udma_EventRxFlowIdFwStatus::chNum

[OUT] The channel index on which the trapped packet was received