AM64x MCU+ SDK  08.05.00
CpswCpts_EstEventMatchParams Struct Reference

Detailed Description

CPTS EST event match params.

Data Fields

Enet_MacPort macPort
 
uint32_t domain
 

Field Documentation

◆ macPort

Enet_MacPort CpswCpts_EstEventMatchParams::macPort

MAC port number

◆ domain

uint32_t CpswCpts_EstEventMatchParams::domain

Domain number of the event. The generated EST events will have the domain set via CpswMacPort_EstTimestampCfg::domain