AM64x MCU+ SDK  08.04.00
Pcie_IbTransCfg Struct Reference

Detailed Description

Inbound traslation configuration info The Pcie_IbTransCfg is used to configure the Inbound Translation Registers.

Data Fields

uint8_t ibBar
 
uint32_t ibStartAddrLo
 
uint32_t ibStartAddrHi
 
uint32_t ibOffsetAddr
 
uint8_t region
 

Field Documentation

◆ ibBar

uint8_t Pcie_IbTransCfg::ibBar

Inbound Translation BAR match

◆ ibStartAddrLo

uint32_t Pcie_IbTransCfg::ibStartAddrLo

Low Inbound Start address (32bits)

◆ ibStartAddrHi

uint32_t Pcie_IbTransCfg::ibStartAddrHi

High Inbound Start address (32bits)

◆ ibOffsetAddr

uint32_t Pcie_IbTransCfg::ibOffsetAddr

Inbound Translation Address Offset (32bits)

◆ region

uint8_t Pcie_IbTransCfg::region

Identifies the translation region (0-3)