AM64x MCU+ SDK  08.04.00
ICSS_EMAC_RxArgument Struct Reference

Detailed Description

Rx packet processing information block that needs to passed into call to ICSS_EMAC_RxPktGet.

Data Fields

ICSS_EMAC_Handle icssEmacHandle
 
uint32_t destAddress
 
uint8_t queueNumber
 
uint8_t port
 
uint32_t more
 

Field Documentation

◆ icssEmacHandle

ICSS_EMAC_Handle ICSS_EMAC_RxArgument::icssEmacHandle

Handle to ICSS_EMAC instance

◆ destAddress

uint32_t ICSS_EMAC_RxArgument::destAddress

Base address of data buffer where received frame has to be stored

◆ queueNumber

uint8_t ICSS_EMAC_RxArgument::queueNumber

Receive queue from which frame has to be copied

◆ port

uint8_t ICSS_EMAC_RxArgument::port

Returns port number on which frame was received

◆ more

uint32_t ICSS_EMAC_RxArgument::more

Returns more which is set to 1 if there are more frames in the queue