AM64x MCU+ SDK  08.04.00
Cpsw_ClearInterVlanRouteUniEgressInArgs Struct Reference

Detailed Description

Data Fields

Cpsw_InterVlanRouteIngressPktMatchCfg inPktMatchCfg
 
Cpsw_InterVlanEgressPortCfg egressCfg
 
uint32_t delAleEntryMask
 

Field Documentation

◆ inPktMatchCfg

Cpsw_InterVlanRouteIngressPktMatchCfg Cpsw_ClearInterVlanRouteUniEgressInArgs::inPktMatchCfg

Ingress packet match criteria for the interVLAN route. If the packet matches the given criteria and the destination port of the packet is host port then the interVLAN route will take effect

◆ egressCfg

Cpsw_InterVlanEgressPortCfg Cpsw_ClearInterVlanRouteUniEgressInArgs::egressCfg

Egress packet modification configuration for the interVLAN route

◆ delAleEntryMask

uint32_t Cpsw_ClearInterVlanRouteUniEgressInArgs::delAleEntryMask

Bitmask to indicate which ALE entries associated with the ingress packet match classifier needs to be deleted

See also
InterVLAN ingress packet match aleEntry delete bitmask