AM64x MCU+ SDK  08.04.00
icss_timeSync.h File Reference

Go to the source code of this file.

Macros

#define TIME_SYNC_OK   (1)
 Success. More...
 
#define TIME_SYNC_UNABLE_TO_CREATE_TASK   (-1)
 Time Sync module is unable to create a Task. More...
 
#define TIME_SYNC_UNABLE_TO_CREATE_SEMAPHORE   (-2)
 Time Sync module is unable to create a Semaphore. More...
 
#define TIME_SYNC_UNABLE_TO_CREATE_INTERRUPT   (-3)
 Time Sync module is unable to create an interrupt. More...
 
#define TIME_SYNC_UNABLE_TO_ALLOC_MEM   (-4)
 Time Sync module is unable to allocate memory. More...
 
#define TIME_SYNC_UNABLE_TO_CREATE_CLOCK   (-5)
 Time Sync module is unable to create timer. More...
 
#define TIME_SYNC_UNABLE_TO_CREATE_MAILBOX   (-6)
 Time Sync module is unable to create a mailbox. More...
 
#define TIME_SYNC_UNABLE_TO_CREATE_EVENT   (-7)
 Time Sync module is unable to create an event. More...
 
#define TIME_SYNC_UNSUPPORTED_FORMAT   (-8)
 Time Sync unsupported format. More...
 
#define TIME_SYNC_EDMA_INIT_FAILED   (-9)
 Time Sync not able to initialize EDMA. More...
 
#define TIME_SYNC_FEATURE_NOT_ENABLED   (-10)
 Time Sync feature disabled. More...
 
#define TIME_SYNC_HANDLE_NOT_INITIALIZED   (-11)
 Time Sync handle uninitialized. More...
 
#define DEFAULT_PDELAY_REQ_LOG_INTERVAL   3
 
#define DEFAULT_SYNC_SEND_LOG_INTERVAL   0
 
#define DEFAULT_ANNOUNCE_SEND_LOG_INTERVAL   1
 
#define DEFAULT_ANNOUNCE_TIMEOUT_LOG_INTERVAL   3
 
#define TIMESYNC_SYNC_ISR_MASK_P1   0x400000
 
#define TIMESYNC_SYNC_ISR_MASK_P2   0x2000000
 
#define TIMESYNC_TX_TS_ISR_MASK_P1   0x800000
 
#define TIMESYNC_TX_TS_ISR_MASK_P2   0x1000000
 
#define PTP_SYNC_MSG_ID   0x00
 
#define PTP_DLY_REQ_MSG_ID   0x01
 
#define PTP_PDLY_REQ_MSG_ID   0x02
 
#define PTP_PDLY_RSP_MSG_ID   0x03
 
#define PTP_FOLLOW_UP_MSG_ID   0x08
 
#define PTP_DLY_RESP_MSG_ID   0x09
 
#define PTP_PDLY_RESP_FLW_UP_MSG_ID   0x0A
 
#define PTP_ANNOUNCE_MSG_ID   0x0B
 
#define PTP_MGMT_MSG_ID   0x0D
 
#define PTP_FLW_UP_CTRL_MSG_ID   0x02
 
#define SEC_TO_NS   1000000000
 
#define FILTER_ALPHA_COEFF   0.85
 
#define PTP_SYNC0_PERIOD_DIVIDER   4
 
#define OFFSET_THRESHOLD_FOR_RESET   10000
 
#define STABLE_FILTER_THRESHOLD   100
 
#define TIMESYNC_PEER_DELAY_ERROR_THRESHOLD   10000
 
#define NUM_SYNC_MISSED_THRESHOLD   3
 
#define AVG_NUM_DELAY_MEASUREMENTS   3
 
#define SRC_MAC_OFFSET   6
 
#define IP_DSCP_OFFSET   15
 
#define SRC_IP_OFFSET   26
 
#define DST_IP_OFFSET   30
 
#define IP_CHKSUM_OFFSET   40
 
#define PTP_MSG_ID_OFFSET   42
 
#define PTP_DOMAIN_NUM_OFFSET   46
 
#define PTP_FLAG_OFFSET   48
 
#define PTP_CORRECTION_OFFSET   50
 
#define PTP_SRC_CLK_IDENTITY   62
 
#define PTP_SRC_PORT_ID_OFFSET   70
 
#define PTP_SEQ_ID_OFFSET   72
 
#define PTP_CONTROL_MSG_ID_OFFSET   74
 
#define PTP_LOG_MSG_PERIOD   75
 
#define PTP_REQ_RCPT_TS_SEC_OFFSET   76
 
#define PTP_REQ_RCPT_TS_NSEC_OFFSET   82
 
#define PTP_REQ_SRC_PORT_IDENTITY   86
 
#define PTP_REQ_SRC_PORT_ID   94
 
#define PTP_UTC_OFFSET   86
 
#define PTP_PRIORITY1_OFFSET   89
 
#define PTP_GM_CLK_CLASS_OFFSET   90
 
#define PTP_GM_CLK_ACCU_OFFSET   91
 
#define PTP_GM_CLK_VARIANCE_OFFSET   92
 
#define PTP_PRIORITY2_OFFSET   94
 
#define PTP_GM_CLK_IDENTITY_OFFSET   95
 
#define PTP_STEPS_REMOVED_OFFSET   103
 
#define PTP_TIME_SRC_OFFSET   105
 
#define PTP_E2E_BUFFER_OFFSET   42
 
#define PTP_P2P_BUFFER_OFFSET   14
 
#define ANNEX_D_ANNEX_F_DIFF   28
 
#define HSR_CORRECTION   6
 
#define SRC_DST_MAC_SIZE   12
 
#define PTP_LEAP_61_MASK   (1<<0)
 
#define PTP_LEAP_59_MASK   (1<<1)
 
#define PTP_UTC_REASONABLE_MASK   (1<<2)
 
#define PTP_TIMESCALE_MASK   (1<<3)
 
#define PTP_TIME_TRACEABLE_MASK   (1<<4)
 
#define PTP_FREQ_TRACEABLE_MASK   (1<<5)
 
#define PTP_ALTERNATE_MASTER_MASK   (1<<8)
 
#define PTP_TWO_STEP_MASK   (1<<9)
 
#define PTP_UNICAST_MASK   (1<<10)
 
#define PTP_PROFILE_SPECIFIC_1_MASK   (1<<13)
 
#define PTP_PROFILE_SPECIFIC_2_MASK   (1<<14)
 
#define PTP_SECURITY_MASK   (1<<15)
 
#define SYNC_INTERVAL_PERIOD_CHANGE_THRESHOLD   60
 
#define GPTP_NUM_DOMAINS   2
 
#define PTP_FLAG_SIZE   (2)
 
#define PTP_SRC_CLK_IDENTITY_SIZE   (8)
 
#define PTP_SRC_PORT_ID_SIZE   (2)
 
#define PTP_GM_CLK_IDENTITY_SIZE   (8)
 
#define PTP_GM_CLK_CLASS_SIZE   (1)
 
#define PTP_GM_CLK_ACCU_SIZE   (1)
 
#define PTP_GM_CLK_VARIANCE_SIZE   (2)
 
#define PTP_UTC_SIZE   (2)
 
#define PTP_TIME_SRC_SIZE   (1)
 
#define PTP_PRIORITY1_SIZE   (1)
 
#define PTP_PRIORITY2_SIZE   (1)
 
#define PTP_STEPS_REMOVED_SIZE   (2)
 

Functions

void TimeSync_resetIEP (TimeSync_ParamsHandle_t timeSyncHandle)
 Resets CMP1 once first adjustment is done, else 1PPS signal doesn't trigger. More...
 
void TimeSync_doFirstAdjustment (TimeSync_ParamsHandle_t timeSyncHandle, uint8_t portNum)
 Do initial adjustment for the IEP based on sync timestamp. More...
 
void TimeSync_Port1linkResetCallBack (uint8_t linkStatus, void *arg2)
 Callback for link status change on Port 1. More...
 
void TimeSync_Port2linkResetCallBack (uint8_t linkStatus, void *arg2)
 Callback for link status change on Port 2. More...
 
void TimeSync_reset (TimeSync_ParamsHandle_t timeSyncHandle)
 Reset the state machine in firmware to restart synchronization (First adjustment happens again) More...
 
void TimeSync_processPTPFrame (TimeSync_ParamsHandle_t timeSyncHandle, uint8_t *pktBuffer, uint8_t portNum, uint16_t size, uint8_t isLinkLocal)
 Processes a PTP message and extract fields. More...
 
uint8_t TimeSync_isEnabled (TimeSync_ParamsHandle_t timeSyncHandle)
 Return True/False 1/0 if timeSync module is enabled. More...
 
void TimeSync_updateParentAddress (TimeSync_ParamsHandle_t timeSyncHandle, uint8_t *parentMac)
 Write the MAC ID of PTP master to Firmware. BMC Algorithm should call this API. More...
 
void TimeSync_getPrevAddress (TimeSync_ParamsHandle_t timeSyncHandle, uint8_t *prevMac)
 Retuns the previous master's MAC ID. More...
 
void TimeSync_getGeneralMessage (TimeSync_ParamsHandle_t timeSyncHandle, int8_t *buff)
 Copies the PTP announce message data to PTP stack buffer. More...
 
void TimeSync_rxPhyDelayCorrection (TimeSync_ParamsHandle_t timeSyncHandle)
 Performs PHY delay correction on Rx timestamp Assumption : The function expects the timestamp in rxTimestamp_gPTP field on which it does correction. More...
 
void TimeSync_getTxTS (TimeSync_ParamsHandle_t timeSyncHandle, uint8_t portNum, ptpFrameTypes_t frameType)
 
void TimeSync_lineDelayCalc (TimeSync_ParamsHandle_t timeSyncHandle)
 
void TimeSync_peerDelayCalc (TimeSync_ParamsHandle_t timeSyncHandle, uint8_t twoStep, uint8_t portNum)
 
void TimeSync_processSyncFrame (TimeSync_ParamsHandle_t timeSyncHandle, uint8_t *buff, uint8_t followUp, uint8_t portNum, uint16_t size)
 
void TimeSync_processDelayResFrame (TimeSync_ParamsHandle_t timeSyncHandle, uint8_t *buff, uint8_t portNum)
 
void TimeSync_processPdelayReqFrame (TimeSync_ParamsHandle_t timeSyncHandle, uint8_t *buff, uint8_t portNum)
 
void TimeSync_processPdelayRespFrame (TimeSync_ParamsHandle_t timeSyncHandle, uint8_t *buff, uint8_t followUp, uint8_t portNum)
 
void TimeSync_forced2StepBDCalc (TimeSync_ParamsHandle_t timeSyncHandle, uint8_t portNum)
 
void TimeSync_synchronizeClock (TimeSync_ParamsHandle_t timeSyncHandle)
 
void TimeSync_calcNRR (TimeSync_ParamsHandle_t timeSyncHandle, uint8_t portNum)
 
void TimeSync_updateNRRParams (TimeSync_ParamsHandle_t timeSyncHandle, uint8_t portNum)
 
void TimeSync_calcRcfAndSyncInterval (TimeSync_ParamsHandle_t timeSyncHandle)
 
void TimeSync_writeTS_SingleStep_Sync (TimeSync_ParamsHandle_t timeSyncHandle, uint8_t portNum)
 
void TimeSync_dummyBMCA (TimeSync_ParamsHandle_t timeSyncHandle, uint8_t *pktBuffer)
 
uint64_t getIEPTimestamp (TimeSync_ParamsHandle_t timeSyncHandle)
 

Macro Definition Documentation

◆ TIME_SYNC_OK

#define TIME_SYNC_OK   (1)

Success.

◆ TIME_SYNC_UNABLE_TO_CREATE_TASK

#define TIME_SYNC_UNABLE_TO_CREATE_TASK   (-1)

Time Sync module is unable to create a Task.

◆ TIME_SYNC_UNABLE_TO_CREATE_SEMAPHORE

#define TIME_SYNC_UNABLE_TO_CREATE_SEMAPHORE   (-2)

Time Sync module is unable to create a Semaphore.

◆ TIME_SYNC_UNABLE_TO_CREATE_INTERRUPT

#define TIME_SYNC_UNABLE_TO_CREATE_INTERRUPT   (-3)

Time Sync module is unable to create an interrupt.

◆ TIME_SYNC_UNABLE_TO_ALLOC_MEM

#define TIME_SYNC_UNABLE_TO_ALLOC_MEM   (-4)

Time Sync module is unable to allocate memory.

◆ TIME_SYNC_UNABLE_TO_CREATE_CLOCK

#define TIME_SYNC_UNABLE_TO_CREATE_CLOCK   (-5)

Time Sync module is unable to create timer.

◆ TIME_SYNC_UNABLE_TO_CREATE_MAILBOX

#define TIME_SYNC_UNABLE_TO_CREATE_MAILBOX   (-6)

Time Sync module is unable to create a mailbox.

◆ TIME_SYNC_UNABLE_TO_CREATE_EVENT

#define TIME_SYNC_UNABLE_TO_CREATE_EVENT   (-7)

Time Sync module is unable to create an event.

◆ TIME_SYNC_UNSUPPORTED_FORMAT

#define TIME_SYNC_UNSUPPORTED_FORMAT   (-8)

Time Sync unsupported format.

◆ TIME_SYNC_EDMA_INIT_FAILED

#define TIME_SYNC_EDMA_INIT_FAILED   (-9)

Time Sync not able to initialize EDMA.

◆ TIME_SYNC_FEATURE_NOT_ENABLED

#define TIME_SYNC_FEATURE_NOT_ENABLED   (-10)

Time Sync feature disabled.

◆ TIME_SYNC_HANDLE_NOT_INITIALIZED

#define TIME_SYNC_HANDLE_NOT_INITIALIZED   (-11)

Time Sync handle uninitialized.

◆ DEFAULT_PDELAY_REQ_LOG_INTERVAL

#define DEFAULT_PDELAY_REQ_LOG_INTERVAL   3

Default PDelay Request packet interval. Actual value is 2^value seconds

◆ DEFAULT_SYNC_SEND_LOG_INTERVAL

#define DEFAULT_SYNC_SEND_LOG_INTERVAL   0

Default Sync transmit interval. Actual value is 2^value seconds

◆ DEFAULT_ANNOUNCE_SEND_LOG_INTERVAL

#define DEFAULT_ANNOUNCE_SEND_LOG_INTERVAL   1

Default Announce packet transmit interval. Actual value is 2^value seconds

◆ DEFAULT_ANNOUNCE_TIMEOUT_LOG_INTERVAL

#define DEFAULT_ANNOUNCE_TIMEOUT_LOG_INTERVAL   3

Default Announce packet timeout. Actual value is 2^value seconds

◆ TIMESYNC_SYNC_ISR_MASK_P1

#define TIMESYNC_SYNC_ISR_MASK_P1   0x400000

Interrupt mask for PRU event 22

◆ TIMESYNC_SYNC_ISR_MASK_P2

#define TIMESYNC_SYNC_ISR_MASK_P2   0x2000000

Interrupt mask for PRU event 25

◆ TIMESYNC_TX_TS_ISR_MASK_P1

#define TIMESYNC_TX_TS_ISR_MASK_P1   0x800000

◆ TIMESYNC_TX_TS_ISR_MASK_P2

#define TIMESYNC_TX_TS_ISR_MASK_P2   0x1000000

Interrupt mask for PRU event 24

◆ PTP_SYNC_MSG_ID

#define PTP_SYNC_MSG_ID   0x00

Sync message ID value

◆ PTP_DLY_REQ_MSG_ID

#define PTP_DLY_REQ_MSG_ID   0x01

Delay request message ID value

◆ PTP_PDLY_REQ_MSG_ID

#define PTP_PDLY_REQ_MSG_ID   0x02

PDelay request message ID value

◆ PTP_PDLY_RSP_MSG_ID

#define PTP_PDLY_RSP_MSG_ID   0x03

PDelay response message ID value

◆ PTP_FOLLOW_UP_MSG_ID

#define PTP_FOLLOW_UP_MSG_ID   0x08

Follow up message ID value

◆ PTP_DLY_RESP_MSG_ID

#define PTP_DLY_RESP_MSG_ID   0x09

Delay response message ID value

◆ PTP_PDLY_RESP_FLW_UP_MSG_ID

#define PTP_PDLY_RESP_FLW_UP_MSG_ID   0x0A

PDelay response follow up message ID value

◆ PTP_ANNOUNCE_MSG_ID

#define PTP_ANNOUNCE_MSG_ID   0x0B

Announce message ID value

◆ PTP_MGMT_MSG_ID

#define PTP_MGMT_MSG_ID   0x0D

Management message ID value

◆ PTP_FLW_UP_CTRL_MSG_ID

#define PTP_FLW_UP_CTRL_MSG_ID   0x02

Control message ID value for Follow Up

◆ SEC_TO_NS

#define SEC_TO_NS   1000000000

Value of seconds in nanoseconds. Useful for calculations

◆ FILTER_ALPHA_COEFF

#define FILTER_ALPHA_COEFF   0.85

Alpha coefficient for sync interval exponential filter and other filters

◆ PTP_SYNC0_PERIOD_DIVIDER

#define PTP_SYNC0_PERIOD_DIVIDER   4

CMP1 period divided by this number makes the width of the Sync pulse

◆ OFFSET_THRESHOLD_FOR_RESET

#define OFFSET_THRESHOLD_FOR_RESET   10000

If offset from Master goes above this threshold it will trigger a reset. Value is in nanoseconds

◆ STABLE_FILTER_THRESHOLD

#define STABLE_FILTER_THRESHOLD   100

When clock drift goes below this value it indicates drift has stabilized and SMA filter can kick in

◆ TIMESYNC_PEER_DELAY_ERROR_THRESHOLD

#define TIMESYNC_PEER_DELAY_ERROR_THRESHOLD   10000

When peer delay exceeds this value it gets reset to 0 Sometimes wrong values are calculated when doing peer delay calculation when clock on peer changes in between peer delay messages and because of the filter this value stays for a long time This helps in fixing it. This is set to a value much higher than max peer delay (of a 100 mtr cable)

◆ NUM_SYNC_MISSED_THRESHOLD

#define NUM_SYNC_MISSED_THRESHOLD   3

If this many consecutive sync frames are missed the DUT gets reset

◆ AVG_NUM_DELAY_MEASUREMENTS

#define AVG_NUM_DELAY_MEASUREMENTS   3

Number of values in the running average

◆ SRC_MAC_OFFSET

#define SRC_MAC_OFFSET   6

Source MAC address offset

◆ IP_DSCP_OFFSET

#define IP_DSCP_OFFSET   15

Differentiated Services Code Point (DSCP) offset in IP4/UDP

◆ SRC_IP_OFFSET

#define SRC_IP_OFFSET   26

Source IP address offset in IP4/UDP

◆ DST_IP_OFFSET

#define DST_IP_OFFSET   30

Destination IP address offset in IP4/UDP

◆ IP_CHKSUM_OFFSET

#define IP_CHKSUM_OFFSET   40

IP4 checksum offset in IP4/UDP

◆ PTP_MSG_ID_OFFSET

#define PTP_MSG_ID_OFFSET   42

PTP message ID offset

◆ PTP_DOMAIN_NUM_OFFSET

#define PTP_DOMAIN_NUM_OFFSET   46

PTP domain number offset

◆ PTP_FLAG_OFFSET

#define PTP_FLAG_OFFSET   48

Offset for PTP flags (including 2 step)

◆ PTP_CORRECTION_OFFSET

#define PTP_CORRECTION_OFFSET   50

Offset for PTP correction field

◆ PTP_SRC_CLK_IDENTITY

#define PTP_SRC_CLK_IDENTITY   62

Offset for PTP source clock identity (MAC + protocol id)

◆ PTP_SRC_PORT_ID_OFFSET

#define PTP_SRC_PORT_ID_OFFSET   70

Offset source port id

◆ PTP_SEQ_ID_OFFSET

#define PTP_SEQ_ID_OFFSET   72

Offset for sequence identifier (incremented every frame)

◆ PTP_CONTROL_MSG_ID_OFFSET

#define PTP_CONTROL_MSG_ID_OFFSET   74

Offset for message id. This categorizes frames into two groups time critical and non time critical

◆ PTP_LOG_MSG_PERIOD

#define PTP_LOG_MSG_PERIOD   75

Log message interval offset

◆ PTP_REQ_RCPT_TS_SEC_OFFSET

#define PTP_REQ_RCPT_TS_SEC_OFFSET   76

Offset for seconds timestamp

◆ PTP_REQ_RCPT_TS_NSEC_OFFSET

#define PTP_REQ_RCPT_TS_NSEC_OFFSET   82

Offset for nanoseconds timestamp

◆ PTP_REQ_SRC_PORT_IDENTITY

#define PTP_REQ_SRC_PORT_IDENTITY   86

Offset for requestor clock identity

◆ PTP_REQ_SRC_PORT_ID

#define PTP_REQ_SRC_PORT_ID   94

Offset for requestor port identity

◆ PTP_UTC_OFFSET

#define PTP_UTC_OFFSET   86

Offset for UTC offset in Announce frame

◆ PTP_PRIORITY1_OFFSET

#define PTP_PRIORITY1_OFFSET   89

Offset for Priority 1 field in Announce frame

◆ PTP_GM_CLK_CLASS_OFFSET

#define PTP_GM_CLK_CLASS_OFFSET   90

Offset for GM clock class field in Announce frame

◆ PTP_GM_CLK_ACCU_OFFSET

#define PTP_GM_CLK_ACCU_OFFSET   91

Offset for GM clock accuracy field in Announce frame

◆ PTP_GM_CLK_VARIANCE_OFFSET

#define PTP_GM_CLK_VARIANCE_OFFSET   92

Offset for GM clock variance field in Announce frame

◆ PTP_PRIORITY2_OFFSET

#define PTP_PRIORITY2_OFFSET   94

Offset for priority 2 field in Announce frame

◆ PTP_GM_CLK_IDENTITY_OFFSET

#define PTP_GM_CLK_IDENTITY_OFFSET   95

Offset for GM clock identity field in Announce frame

◆ PTP_STEPS_REMOVED_OFFSET

#define PTP_STEPS_REMOVED_OFFSET   103

Offset for steps removed field in Announce frame

◆ PTP_TIME_SRC_OFFSET

#define PTP_TIME_SRC_OFFSET   105

Offset for GM time source field in Announce frame

◆ PTP_E2E_BUFFER_OFFSET

#define PTP_E2E_BUFFER_OFFSET   42

Offset for start of PTP data in UDP/IP4 frame

◆ PTP_P2P_BUFFER_OFFSET

#define PTP_P2P_BUFFER_OFFSET   14

Offset for start of PTP data in 802.3 frame

◆ ANNEX_D_ANNEX_F_DIFF

#define ANNEX_D_ANNEX_F_DIFF   28

Number of Extra bytes from Annex F(802.1) to Annex E(UDP)

◆ HSR_CORRECTION

#define HSR_CORRECTION   6

Number of bytes in HSR Header

◆ SRC_DST_MAC_SIZE

#define SRC_DST_MAC_SIZE   12

Num bytes in source plus destination MAC

◆ PTP_LEAP_61_MASK

#define PTP_LEAP_61_MASK   (1<<0)

Mask for Leap 61 status in PTP Flags

◆ PTP_LEAP_59_MASK

#define PTP_LEAP_59_MASK   (1<<1)

Mask for Leap 59 status in PTP Flags

◆ PTP_UTC_REASONABLE_MASK

#define PTP_UTC_REASONABLE_MASK   (1<<2)

Mask for UTC reasonable value in PTP Flags

◆ PTP_TIMESCALE_MASK

#define PTP_TIMESCALE_MASK   (1<<3)

Mask for value indicating whether PTP Timescale in PTP Flags

◆ PTP_TIME_TRACEABLE_MASK

#define PTP_TIME_TRACEABLE_MASK   (1<<4)

Mask for value indicating whether time traceable in PTP Flags

◆ PTP_FREQ_TRACEABLE_MASK

#define PTP_FREQ_TRACEABLE_MASK   (1<<5)

Mask for value indicating whether freq traceable in PTP Flags

◆ PTP_ALTERNATE_MASTER_MASK

#define PTP_ALTERNATE_MASTER_MASK   (1<<8)

Mask for value indicating whether alternate master in PTP Flags

◆ PTP_TWO_STEP_MASK

#define PTP_TWO_STEP_MASK   (1<<9)

Mask for value indicating whether two step sync in PTP Flags

◆ PTP_UNICAST_MASK

#define PTP_UNICAST_MASK   (1<<10)

Mask for value indicating whether messaging is unicast in PTP Flags

◆ PTP_PROFILE_SPECIFIC_1_MASK

#define PTP_PROFILE_SPECIFIC_1_MASK   (1<<13)

Mask for value indicating alternate PTP Profile in PTP Flags

◆ PTP_PROFILE_SPECIFIC_2_MASK

#define PTP_PROFILE_SPECIFIC_2_MASK   (1<<14)

Mask for value indicating alternate PTP Profile in PTP Flags

◆ PTP_SECURITY_MASK

#define PTP_SECURITY_MASK   (1<<15)

Mask for value indicating whether PTP security is enabled or not in PTP Flags

◆ SYNC_INTERVAL_PERIOD_CHANGE_THRESHOLD

#define SYNC_INTERVAL_PERIOD_CHANGE_THRESHOLD   60

If current sync interval varies from previously measured sync interval by this much percentage then it triggers a PTP reset

◆ GPTP_NUM_DOMAINS

#define GPTP_NUM_DOMAINS   2

Number of domains supported by GPTP implementation

◆ PTP_FLAG_SIZE

#define PTP_FLAG_SIZE   (2)

Size for PTP flags (including 2 step)

◆ PTP_SRC_CLK_IDENTITY_SIZE

#define PTP_SRC_CLK_IDENTITY_SIZE   (8)

Size for PTP source clock identity (MAC + protocol id)

◆ PTP_SRC_PORT_ID_SIZE

#define PTP_SRC_PORT_ID_SIZE   (2)

Size for source port id field

◆ PTP_GM_CLK_IDENTITY_SIZE

#define PTP_GM_CLK_IDENTITY_SIZE   (8)

Size for GM clock identity field in Announce frame

◆ PTP_GM_CLK_CLASS_SIZE

#define PTP_GM_CLK_CLASS_SIZE   (1)

Size for GM clock class field in Announce frame

◆ PTP_GM_CLK_ACCU_SIZE

#define PTP_GM_CLK_ACCU_SIZE   (1)

Size for GM clock accuracy field in Announce frame

◆ PTP_GM_CLK_VARIANCE_SIZE

#define PTP_GM_CLK_VARIANCE_SIZE   (2)

Size for GM clock variance field in Announce frame

◆ PTP_UTC_SIZE

#define PTP_UTC_SIZE   (2)

Size for UTC offset in Announce frame

◆ PTP_TIME_SRC_SIZE

#define PTP_TIME_SRC_SIZE   (1)

Size for GM time source field in Announce frame

◆ PTP_PRIORITY1_SIZE

#define PTP_PRIORITY1_SIZE   (1)

Size for Priority 1 field in Announce frame

◆ PTP_PRIORITY2_SIZE

#define PTP_PRIORITY2_SIZE   (1)

Size for Priority 2 field in Announce frame

◆ PTP_STEPS_REMOVED_SIZE

#define PTP_STEPS_REMOVED_SIZE   (2)

Offset for steps removed field in Announce frame

Function Documentation

◆ TimeSync_resetIEP()

void TimeSync_resetIEP ( TimeSync_ParamsHandle_t  timeSyncHandle)

Resets CMP1 once first adjustment is done, else 1PPS signal doesn't trigger.

Parameters
timeSyncHandlepointer to PTP Handle structure

◆ TimeSync_doFirstAdjustment()

void TimeSync_doFirstAdjustment ( TimeSync_ParamsHandle_t  timeSyncHandle,
uint8_t  portNum 
)

Do initial adjustment for the IEP based on sync timestamp.

Parameters
timeSyncHandlepointer to PTP Handle structure
portNumICSS_EMAC_PORT_1 or ICSS_EMAC_PORT_2

◆ TimeSync_getTxTS()

void TimeSync_getTxTS ( TimeSync_ParamsHandle_t  timeSyncHandle,
uint8_t  portNum,
ptpFrameTypes_t  frameType 
)

◆ TimeSync_lineDelayCalc()

void TimeSync_lineDelayCalc ( TimeSync_ParamsHandle_t  timeSyncHandle)

◆ TimeSync_peerDelayCalc()

void TimeSync_peerDelayCalc ( TimeSync_ParamsHandle_t  timeSyncHandle,
uint8_t  twoStep,
uint8_t  portNum 
)

◆ TimeSync_processSyncFrame()

void TimeSync_processSyncFrame ( TimeSync_ParamsHandle_t  timeSyncHandle,
uint8_t *  buff,
uint8_t  followUp,
uint8_t  portNum,
uint16_t  size 
)

◆ TimeSync_processDelayResFrame()

void TimeSync_processDelayResFrame ( TimeSync_ParamsHandle_t  timeSyncHandle,
uint8_t *  buff,
uint8_t  portNum 
)

◆ TimeSync_processPdelayReqFrame()

void TimeSync_processPdelayReqFrame ( TimeSync_ParamsHandle_t  timeSyncHandle,
uint8_t *  buff,
uint8_t  portNum 
)

◆ TimeSync_processPdelayRespFrame()

void TimeSync_processPdelayRespFrame ( TimeSync_ParamsHandle_t  timeSyncHandle,
uint8_t *  buff,
uint8_t  followUp,
uint8_t  portNum 
)

◆ TimeSync_forced2StepBDCalc()

void TimeSync_forced2StepBDCalc ( TimeSync_ParamsHandle_t  timeSyncHandle,
uint8_t  portNum 
)

◆ TimeSync_synchronizeClock()

void TimeSync_synchronizeClock ( TimeSync_ParamsHandle_t  timeSyncHandle)

◆ TimeSync_calcNRR()

void TimeSync_calcNRR ( TimeSync_ParamsHandle_t  timeSyncHandle,
uint8_t  portNum 
)

◆ TimeSync_updateNRRParams()

void TimeSync_updateNRRParams ( TimeSync_ParamsHandle_t  timeSyncHandle,
uint8_t  portNum 
)

◆ TimeSync_calcRcfAndSyncInterval()

void TimeSync_calcRcfAndSyncInterval ( TimeSync_ParamsHandle_t  timeSyncHandle)

◆ TimeSync_writeTS_SingleStep_Sync()

void TimeSync_writeTS_SingleStep_Sync ( TimeSync_ParamsHandle_t  timeSyncHandle,
uint8_t  portNum 
)

◆ TimeSync_dummyBMCA()

void TimeSync_dummyBMCA ( TimeSync_ParamsHandle_t  timeSyncHandle,
uint8_t *  pktBuffer 
)

◆ getIEPTimestamp()

uint64_t getIEPTimestamp ( TimeSync_ParamsHandle_t  timeSyncHandle)