AM64x MCU+ SDK  08.04.00

Introduction

Functions

void bsp_eeprom_emulation_init (void)
 Initialize the EEPROM cache in volatile RAM. If the non-volatile storage has valid data(read is performed using eeprom_read callback from bsp_params passed during bsp_init), load from there. Otherwise it loads predefined EEPROM in application using default_tiesc_eeprom from bsp_params passed during bsp_init. More...
 
int32_t bsp_eeprom_load_esc_registers (PRUICSS_Handle pruIcssHandle, int32_t reload_flag)
 For loading ESC registers from EEPROM during first boot/reload after validating CRC. More...
 
int32_t bsp_eeprom_emulation_reload (PRUICSS_Handle pruIcssHandle)
 Perform reload operation after validating EEPROM CRC. More...
 
void bsp_eeprom_emulation_command_ack (PRUICSS_Handle pruIcssHandle)
 Perform reload operation after validating EEPROM CRC, Wrapper API for SSC. More...
 
void bsp_eeprom_emulation_flush (void)
 Flush the EEPROM cache to non-volatile storage. Write is performed using eeprom_write callback from bsp_params passed during bsp_init. More...
 
void bsp_eeprom_emulation_exit (void)
 Call EEPROM flush on exit. More...
 
uint8_t * bsp_get_eeprom_cache_base (void)
 Return pointer to volatile EEPROM cache in FWHAL for processing to access the EEPROM. More...
 
void bsp_set_eeprom_updated_time (void)
 Set EEPROM update time. More...
 
uint32_t bsp_get_eeprom_updated_time (void)
 Get EEPROM Updated time. More...
 
void bsp_set_eeprom_update_status (uint8_t status)
 Indicate to FWHAL whether EEPROM is written for flushing to non-volatile storage. Typically called on EEPROM write detection from stack. More...
 
uint8_t bsp_get_eeprom_update_status (void)
 Read the EEPROM update status from FWHAL. Typically called from low priority task periodically check EEPROM dirty status for flush. More...
 

Function Documentation

◆ bsp_eeprom_emulation_init()

void bsp_eeprom_emulation_init ( void  )

Initialize the EEPROM cache in volatile RAM. If the non-volatile storage has valid data(read is performed using eeprom_read callback from bsp_params passed during bsp_init), load from there. Otherwise it loads predefined EEPROM in application using default_tiesc_eeprom from bsp_params passed during bsp_init.

◆ bsp_eeprom_load_esc_registers()

int32_t bsp_eeprom_load_esc_registers ( PRUICSS_Handle  pruIcssHandle,
int32_t  reload_flag 
)

For loading ESC registers from EEPROM during first boot/reload after validating CRC.

Parameters
pruIcssHandlePRUSS handle
reload_flagIf set reload command is being executed else first boot in progress
Return values
0On successful load of registers -1: On CRC error

◆ bsp_eeprom_emulation_reload()

int32_t bsp_eeprom_emulation_reload ( PRUICSS_Handle  pruIcssHandle)

Perform reload operation after validating EEPROM CRC.

Parameters
pruIcssHandlePRUSS handle
Return values
0On successful load of registers -1: On CRC error

◆ bsp_eeprom_emulation_command_ack()

void bsp_eeprom_emulation_command_ack ( PRUICSS_Handle  pruIcssHandle)

Perform reload operation after validating EEPROM CRC, Wrapper API for SSC.

Parameters
pruIcssHandlePRUSS handle

◆ bsp_eeprom_emulation_flush()

void bsp_eeprom_emulation_flush ( void  )

Flush the EEPROM cache to non-volatile storage. Write is performed using eeprom_write callback from bsp_params passed during bsp_init.

◆ bsp_eeprom_emulation_exit()

void bsp_eeprom_emulation_exit ( void  )

Call EEPROM flush on exit.

◆ bsp_get_eeprom_cache_base()

uint8_t* bsp_get_eeprom_cache_base ( void  )

Return pointer to volatile EEPROM cache in FWHAL for processing to access the EEPROM.

Return values
Pointerto volatile EEPROM cache start to the stack/application for EEPROM access

◆ bsp_set_eeprom_updated_time()

void bsp_set_eeprom_updated_time ( void  )

Set EEPROM update time.

◆ bsp_get_eeprom_updated_time()

uint32_t bsp_get_eeprom_updated_time ( void  )

Get EEPROM Updated time.

Return values
EEPROMupdated time

◆ bsp_set_eeprom_update_status()

void bsp_set_eeprom_update_status ( uint8_t  status)

Indicate to FWHAL whether EEPROM is written for flushing to non-volatile storage. Typically called on EEPROM write detection from stack.

Parameters
statusUpdate the FWHAL EEPROM update status.

◆ bsp_get_eeprom_update_status()

uint8_t bsp_get_eeprom_update_status ( void  )

Read the EEPROM update status from FWHAL. Typically called from low priority task periodically check EEPROM dirty status for flush.

Return values
EEPROMupdated status