AM64x MCU+ SDK  08.04.00

Introduction

See IPC RPMessage for more details.

Data Structures

struct  RPMessage_Object
 Opaque RPMessage object used with the RPMessage APIs. More...
 
struct  RPMessage_CreateParams
 Parameters passed to RPMessage_construct. More...
 
struct  RPMessage_Params
 Parameters passed to RPMessage_init, these are generated via SysCfg. More...
 

Functions

void RPMessage_Params_init (RPMessage_Params *params)
 Set default values to RPMessage_Params. More...
 
void RPMessage_CreateParams_init (RPMessage_CreateParams *params)
 Set default values to RPMessage_CreateParams. More...
 
int32_t RPMessage_init (const RPMessage_Params *params)
 Initialize RPMessage module. More...
 
void RPMessage_deInit ()
 De-Initialize RPMessage module. More...
 
int32_t RPMessage_waitForLinuxReady (uint32_t timeout)
 Wait for linux side RPMessage to be ready. More...
 
void RPMessage_controlEndPtCallback (RPMessage_ControlEndPtCallback controlEndPtCallback, void *controlEndPtCallbackArgs)
 Callback to call when a control message is received on a control end point. More...
 
int32_t RPMessage_construct (RPMessage_Object *obj, const RPMessage_CreateParams *createParams)
 Create a RPMessage object to receive messages at a specified end-point. More...
 
void RPMessage_destruct (RPMessage_Object *obj)
 Delete a previously created RPMessage object. More...
 
void RPMessage_unblock (RPMessage_Object *obj)
 Unblocks RPMessage_recv, for the input object, if it is blocked waiting on messages and users want to exit that task. More...
 
uint16_t RPMessage_getLocalEndPt (const RPMessage_Object *obj)
 Return local end point of a RPMessage_Object. More...
 
int32_t RPMessage_announce (uint16_t remoteProcId, uint16_t localEndPt, const char *name)
 Announce a local end point at which a service is created to a remote core. More...
 
int32_t RPMessage_send (void *data, uint16_t dataLen, uint16_t remoteCoreId, uint16_t remoteEndPt, uint16_t localEndPt, uint32_t timeout)
 Send a message to a remote core at a specified remote end point. More...
 
int32_t RPMessage_recv (RPMessage_Object *obj, void *data, uint16_t *dataLen, uint16_t *remoteCoreId, uint16_t *remoteEndPt, uint32_t timeout)
 Blocking API to wait till a message is received from any CPU at the specified local end point. More...
 

Typedefs

typedef void(* RPMessage_RecvCallback) (RPMessage_Object *obj, void *arg, void *data, uint16_t dataLen, uint16_t remoteCoreId, uint16_t remoteEndPt)
 Callback that is invoked when a message is received from any CPU at the specified local end point. More...
 
typedef void(* RPMessage_RecvNotifyCallback) (RPMessage_Object *obj, void *arg)
 Callback that is invoked when a message is received from any CPU at the specified local end point. More...
 
typedef void(* RPMessage_ControlEndPtCallback) (void *arg, uint16_t remoteCoreId, uint16_t remoteEndPt, const char *remoteServiceName)
 Callback that is invoked when a annoucement message is received on the control end point. More...
 

Macros

#define RPMESSAGE_MAX_LOCAL_ENDPT   (64U)
 Users can create RPMessage_Object with local end value in the range of 0 .. RPMESSAGE_MAX_LOCAL_ENDPT - 1. More...
 
#define RPMESSAGE_VRING_ADDR_INVALID   (0xFFFFFFFFU)
 Value to indicate if vring ID is valid or NOT. More...
 
#define RPMESSAGE_VRING_SIZE(numBuf, bufSize)   (((numBuf)*((bufSize)+32U))+32)
 Returns the size needed for each VRING. More...
 
#define RPMESSAGE_OBJECT_SIZE_MAX   (192U)
 Size of RPMessage_Object. More...
 

Macro Definition Documentation

◆ RPMESSAGE_MAX_LOCAL_ENDPT

#define RPMESSAGE_MAX_LOCAL_ENDPT   (64U)

Users can create RPMessage_Object with local end value in the range of 0 .. RPMESSAGE_MAX_LOCAL_ENDPT - 1.

This limit is put to allow fast indexing of end point object to recevied messages and the value is kept small to save memory space

◆ RPMESSAGE_VRING_ADDR_INVALID

#define RPMESSAGE_VRING_ADDR_INVALID   (0xFFFFFFFFU)

Value to indicate if vring ID is valid or NOT.

When a core does not participate in IPC RPMessage set the vring ID in RPMessage_Params to this value

◆ RPMESSAGE_VRING_SIZE

#define RPMESSAGE_VRING_SIZE (   numBuf,
  bufSize 
)    (((numBuf)*((bufSize)+32U))+32)

Returns the size needed for each VRING.

This is approximate size that is >= to actual required size. Approximate size is returned to allow compile time macro for size calculation. Actual required size is calculated in the internal run-time function RPMessage_vringGetSize. However this can be ignored by end users. During initialization, a assert is used to check if user provided size is >= actual required size.

Parameters
numBuf[in] Number of buffer in the VRING
bufSize[in] Size of each buffer, in units of bytes
Returns
VRING size in bytes

◆ RPMESSAGE_OBJECT_SIZE_MAX

#define RPMESSAGE_OBJECT_SIZE_MAX   (192U)

Size of RPMessage_Object.

Typedef Documentation

◆ RPMessage_RecvCallback

typedef void(* RPMessage_RecvCallback) (RPMessage_Object *obj, void *arg, void *data, uint16_t dataLen, uint16_t remoteCoreId, uint16_t remoteEndPt)

Callback that is invoked when a message is received from any CPU at the specified local end point.

The callback can be optionally registered during RPMessage_construct

Note
All message contents MUST be consumed in the callback. When callback returns the message buffer is released back to the sender. If the message contents are needed for deferred processing then take a copy of the message contents
Parameters
obj[in] RPMessage end point object created with RPMessage_construct
arg[in] Arguments specified by user during RPMessage_construct
data[in] Pointer to message
dataLen[in] Length of message
remoteCoreId[in] Core ID of sender
remoteEndPt[in] End point of sender

◆ RPMessage_RecvNotifyCallback

typedef void(* RPMessage_RecvNotifyCallback) (RPMessage_Object *obj, void *arg)

Callback that is invoked when a message is received from any CPU at the specified local end point.

The callback can be optionally registered during RPMessage_construct

Note
Unlike RPMessage_RecvCallback, this callback only notifies that there is one or more messages to be read, but the message itself is not read by the driver unless RPMessage_recv is called in this callback or later within a task.
If RPMessage_RecvCallback is set, then RPMessage_RecvNotifyCallback callback is not used.
Parameters
obj[in] RPMessage end point object created with RPMessage_construct
arg[in] Arguments specified by user during RPMessage_construct

◆ RPMessage_ControlEndPtCallback

typedef void(* RPMessage_ControlEndPtCallback) (void *arg, uint16_t remoteCoreId, uint16_t remoteEndPt, const char *remoteServiceName)

Callback that is invoked when a annoucement message is received on the control end point.

The callback can be optionally registered during RPMessage_init

Note
All message contents MUST be consumed in the callback. When callback returns the message buffer is released back to the sender. If the message contents are needed for deferred processing then take a copy of the message contents
Parameters
arg[in] Arguments specified by user during RPMessage_init
remoteCoreId[in] Core ID of sender
remoteEndPt[in] End point of sender that has annoucned the service over the control end point
remoteServiceName[in] Name of the remote service that is annoucned

Function Documentation

◆ RPMessage_Params_init()

void RPMessage_Params_init ( RPMessage_Params params)

Set default values to RPMessage_Params.

Parameters
params[out] default intialized structure

◆ RPMessage_CreateParams_init()

void RPMessage_CreateParams_init ( RPMessage_CreateParams params)

Set default values to RPMessage_CreateParams.

Parameters
params[out] default intialized structure

◆ RPMessage_init()

int32_t RPMessage_init ( const RPMessage_Params params)

Initialize RPMessage module.

Parameters
params[in] Initialization parameters

◆ RPMessage_deInit()

void RPMessage_deInit ( )

De-Initialize RPMessage module.

◆ RPMessage_waitForLinuxReady()

int32_t RPMessage_waitForLinuxReady ( uint32_t  timeout)

Wait for linux side RPMessage to be ready.

Messages should not be sent to Linux, if enabled, until this function return success.

Note
When using RPMessage between RTOS/no-RTOS cores then this API needed not be called.
Parameters
timeout[in] Timeout in units of system ticks
Returns
SystemP_SUCCESS, linux has initialized its side of RPMessage

◆ RPMessage_controlEndPtCallback()

void RPMessage_controlEndPtCallback ( RPMessage_ControlEndPtCallback  controlEndPtCallback,
void *  controlEndPtCallbackArgs 
)

Callback to call when a control message is received on a control end point.

Parameters
controlEndPtCallback[in] User callback to invoke
controlEndPtCallbackArgs[in] Arguments pass to the user control end point callback

◆ RPMessage_construct()

int32_t RPMessage_construct ( RPMessage_Object obj,
const RPMessage_CreateParams createParams 
)

Create a RPMessage object to receive messages at a specified end-point.

Note
Each new object that is created MUST have a unique local end point.
Local end point MUST be < RPMESSAGE_MAX_LOCAL_ENDPT
User MUST choose a value and ANY is not supported
When callback is registered in RPMessage_CreateParams, RPMessage_recv MUST not be used.
Parameters
obj[out] Created object
createParams[in] parameters
Returns
SystemP_SUCCESS on success, else failure.

◆ RPMessage_destruct()

void RPMessage_destruct ( RPMessage_Object obj)

Delete a previously created RPMessage object.

Parameters
obj[in] object

◆ RPMessage_unblock()

void RPMessage_unblock ( RPMessage_Object obj)

Unblocks RPMessage_recv, for the input object, if it is blocked waiting on messages and users want to exit that task.

Parameters
obj[in] object

◆ RPMessage_getLocalEndPt()

uint16_t RPMessage_getLocalEndPt ( const RPMessage_Object obj)

Return local end point of a RPMessage_Object.

The value will be same as that was used to create the object earlier.

Parameters
obj[in] object
Returns
local end point of input object

◆ RPMessage_announce()

int32_t RPMessage_announce ( uint16_t  remoteProcId,
uint16_t  localEndPt,
const char *  name 
)

Announce a local end point at which a service is created to a remote core.

Note
Announcing end points is optional and is not used internally by IPC RPmessage in any way.
User MUST announce one by one to all remote core's of interest. There is no announce to ALL option
To handle announcement messages, make sure user handler is registered during RPMessage_init via RPMessage_Params
It is upto the end user to use the callback to signal or wait until a remote service is announced.
Parameters
remoteProcId[in] The remote core to annouce to.
localEndPt[in] Local end point of the service that is being announced
name[in] Name of the service that is being announced
Returns
SystemP_SUCCESS, when the annouce message was sent, else failure

◆ RPMessage_send()

int32_t RPMessage_send ( void *  data,
uint16_t  dataLen,
uint16_t  remoteCoreId,
uint16_t  remoteEndPt,
uint16_t  localEndPt,
uint32_t  timeout 
)

Send a message to a remote core at a specified remote end point.

Note
dataLen MUST be <= RPMessage_Params::vringMsgSize - 16 bytes for internal header
In order for a remote core to receive the message, a end point should be created on the remote core at the same value as remoteEndPt
localEndPt, is strictly not needed, however this is available to the user on the remote core and can be used as a reply end point. Use RPMessage_getLocalEndPt to set to the RPMessage object at which to listen for replies
When timeout is 0, then if a free buffer is not available to transmit, it will return will immediately SystemP_TIMEOUT. Else it will wait for specified timeout ticks for a free buffer to be available.
Parameters
data[in] Pointer to message data to send
dataLen[in] size of message data to send
remoteCoreId[in] Remote core ID to whom the message is being sent
remoteEndPt[in] Remote core end point ID to which the message is being sent
localEndPt[in] Local end point that is sending the message
timeout[in] Amount of time to wait, in units of system ticks
Returns
SystemP_SUCCESS, when the send message was successful
SystemP_TIMEOUT, message not sent since free transmit buffer not available and timeout happened.

◆ RPMessage_recv()

int32_t RPMessage_recv ( RPMessage_Object obj,
void *  data,
uint16_t *  dataLen,
uint16_t *  remoteCoreId,
uint16_t *  remoteEndPt,
uint32_t  timeout 
)

Blocking API to wait till a message is received from any CPU at the specified local end point.

Note
Local end point is specified during RPMessage_construct
When callback is registered this API should not be used.
dataLen when passed by user contains the user message buffer size, i.e size of buffer pointer to by 'data`. If received message size exceeds *dataLen then it is truncated. If received message size is <= *dataLen then all received bytes are copied to data and *dataLen indicates the size of valid bytes in data
Parameters
obj[in] RPMessage end point object created with RPMessage_construct
data[in] Pointer to received message contents
dataLen[in] Length of user message buffer, in bytes
[out] Size of received message, in bytes
remoteCoreId[out] Core ID of sender
remoteEndPt[out] End point of sender
timeout[in] Time in system ticks to block for a message receive
Returns
SystemP_SUCCESS, new message received, all output parameters are valid
SystemP_TIMEOUT, API unblocked due to timeout and output parameters should not be used.