PROFINET Device  v2.01.00
PN_API_SNMP_SConfiguration Struct Reference

#include <PN_API_SNMP.h>

Data Fields

uint16_t interfaceDescriptionLength
 
uint8_t * pInterfaceDescription
 
uint16_t port1DescriptionLength
 
uint8_t * pPort1Description
 
uint16_t port2DescriptionLength
 
uint8_t * pPort2Description
 
PN_API_SNMP_SPermanentData_tpPermanentData
 
PN_API_SNMP_SCallbacks_t callBacks