PROFINET Device  v2.01.00
PN_API_PDEV_SChassisId Struct Reference

#include <PN_API_PDEV.h>

Data Fields

uint16_t deviceDescriptionLength
 
uint8_t * pDeviceDescription
 
uint16_t orderIdLength
 
uint8_t * pOrderId
 
uint16_t serialNumberLength
 
uint8_t * pSerialNumber
 
uint16_t hwRevisionLength
 
uint8_t * pHwRevision
 
uint8_t swRevisionPrefix
 
uint16_t swRevisionFunctionalEnhancementLength
 
uint8_t * pSwRevisionFunctionalEnhancement
 
uint16_t swRevisionBugFixLength
 
uint8_t * pSwRevisionBugFix
 
uint16_t swRevisionInternalChangeLength
 
uint8_t * pSwRevisionInternalChange