PROFINET Device
v2.01.00
◆
PN_API_SNMP_applyConfiguration()
uint32_t PN_API_SNMP_applyConfiguration
(
const
PN_API_SNMP_SConfiguration_t
*
pConfiguration_p
)
Apply SNMP configuration.
ToDo.
Remarks
ToTo or remove tag.
Parameters
[in]
pConfiguration_p
Pointer to SNMP configuration.
Returns
#PN_API_SNMP_error_t as uint32_t
Return values
#PN_API_SNMP_OK
Example
#include <PN_API_SNMP.h>
See also
PN_API_PDEV_start
PN_API_PDEV_run
Simple Network Management Protocol
generated by
1.8.17