EtherNet/IP™ Adapter  1.04.10
User Reference Manual

◆ EI_API_ADP_setPortLogAnnounceInterval()

uint32_t EI_API_ADP_setPortLogAnnounceInterval ( T pAdp_p,
uint16_t  portLogAnnounceInterval_p 
)

Set the PortLogAnnounceInterval of the Time Sync object of the adapter (Instance Attribute ID: 14).

Function that sets the member in the PortLogAnnounceIntervalCfg attribute of the adapter selected by parameter pAdp_p. PortLogAnnounceInterval specifies the PTP announce interval between successive Announce messages issued by a master clock on each PTP port of the device. The units of the PortLogAnnounceInterval member are log base 2 seconds. The data type of the PortLogAnnounceInterval is uint16_t. The permitted value range is between 0 and 4.

Parameters
[in]pAdp_pPointer to the adapter.
[in]portLogAnnounceInterval_puint16_t Value of PTP Announce frame interval.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
// Set portLogAnnounceInterval in Time Sync object
uint16_t portLogAnnounceInterval = 1;
errCode = EI_API_ADP_setPortLogAnnounceInterval(pEI_API_ADP, portLogAnnounceInterval);
See also
EI_API_ADP_getPortLogAnnounceInterval EI_API_ADP_EError_t
EI_API_ADP_setPortLogAnnounceInterval
ETHIP_API uint32_t EI_API_ADP_setPortLogAnnounceInterval(T *pAdp_p, uint16_t portLogAnnounceInterval_p)
Set the PortLogAnnounceInterval of the Time Sync object of the adapter (Instance Attribute ID: 14).
Definition: EI_API_ADP_main.c:2270
EI_API_ADP_new
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:285