EtherNet/IP™ Adapter  1.04.10
User Reference Manual

◆ EI_API_ADP_getTimeSyncUserDescription()

uint32_t EI_API_ADP_getTimeSyncUserDescription ( T pAdp_p,
char *  pUserDescription_p 
)

Get the Description member of the UserDescription attribute of the Time Sync object (Instance Attribute ID: 23).

Function that returns the Description member of the UserDescription attribute for the adapter sleected by parameter pAdp_p in output parameter pUserDescription_p.

Parameters
[in]pAdp_pPointer to the adapter.
[out]pUserDescription_pchar pointer to UserDescription of the adapter Time Sync object specified by parameter pAdp_p.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
char userDescription[128];
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
errCode = EI_API_ADP_getTimeSyncUserDescription(pEI_API_ADP, userDescription);
See also
EI_API_ADP_setTimeSyncUserDescription EI_API_ADP_EError_t
EI_API_ADP_getTimeSyncUserDescription
ETHIP_API uint32_t EI_API_ADP_getTimeSyncUserDescription(T *pAdp_p, char *pUserDescription_p)
Get the Description member of the UserDescription attribute of the Time Sync object (Instance Attribu...
Definition: EI_API_ADP_main.c:3099
EI_API_ADP_new
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:285