EtherNet/IP™ Adapter  1.04.10
User Reference Manual

◆ EI_API_ADP_setDomainNumber()

uint32_t EI_API_ADP_setDomainNumber ( T pAdp_p,
uint8_t  domainNumber_p 
)

Set the DomainNumber attribute of the Time Sync object of the adapter (Instance Attribute ID: 18).

Function that sets the DomainNumber attribute of the Time Sync object of the adapter selected by parameter pAdp_p. DomainNumber specifies the PTP clock domain. The datatype of DomainNumber is uint8_t. The permitted value range is between 0 and 127.

Parameters
[in]pAdp_pPointer to the adapter.
[in]domainNumber_puint8_t Domain number.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
// Set DomainNumber in timeSync object
uint8_t domainNumber = 0;
errCode = EI_API_ADP_setDomainNumber(pEI_API_ADP, domainNumber);
See also
EI_API_ADP_getDomainNumber EI_API_ADP_EError_t
EI_API_ADP_setDomainNumber
ETHIP_API uint32_t EI_API_ADP_setDomainNumber(T *pAdp_p, uint8_t domainNumber_p)
Set the DomainNumber attribute of the Time Sync object of the adapter (Instance Attribute ID: 18).
Definition: EI_API_ADP_main.c:2545
EI_API_ADP_new
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:285