EtherNet/IP™ Adapter  1.04.10
User Reference Manual

◆ EI_API_ADP_getEnipAcdHdr()

uint32_t EI_API_ADP_getEnipAcdHdr ( T pAdp_p,
EI_API_ADP_SParam_t pEnipAcdHdr_p 
)

Get the adapter address conflict detection header (Instance Attribute ID: 11).

Function to get the current Address Conflict Detection (ACD) header.

Parameters
[in]pAdp_pPointer to the adapter.
[out]pEnipAcdHdr_pPointer to the ACD header packed within a EI_API_ADP_SParam_t type.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
errCode = EI_API_ADP_getEnipAcdHdr(pEI_API_CIP_ADP, &enipAcdHdr);
See also
EI_API_ADP_setEnipAcdHdr EI_API_ADP_SParam_t EI_API_ADP_EError_t
EI_API_ADP_getEnipAcdHdr
ETHIP_API uint32_t EI_API_ADP_getEnipAcdHdr(T *pAdp_p, EI_API_ADP_SParam_t *pEnipAcdHdr_p)
Get the adapter address conflict detection header (Instance Attribute ID: 11).
Definition: EI_API_ADP_main.c:4828
EI_API_ADP_SParam
Definition: EI_API_ADP.h:117
EI_API_ADP_new
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:285