EtherNet/IP™ Adapter  1.04.10
User Reference Manual

◆ EI_API_ADP_getVendorId()

uint32_t EI_API_ADP_getVendorId ( T pAdp_p,
uint16_t *  pVendorId_p 
)

Get the adapter Vendor ID (Instance Attribute ID: 1).

Function that returns the vendor identifier as uint16_t value for the adapter selected by parameter pAdp_p.

Parameters
[in]pAdp_pPointer to the adapter.
[out]pVendorId_pPointer to the vendor ID.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
uint16_t vendorId;
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
errCode = EI_API_ADP_getVendorId(pEI_API_ADP, &vendorId);
See also
EI_API_ADP_setVendorId EI_API_ADP_EError_t
EI_API_ADP_getVendorId
ETHIP_API uint32_t EI_API_ADP_getVendorId(T *pAdp_p, uint16_t *pVendorId_p)
Get the adapter Vendor ID (Instance Attribute ID: 1).
Definition: EI_API_ADP_main.c:985
EI_API_ADP_new
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:285