EtherCAT Slave  1.08.00

◆ EC_API_SLV_notificationResponse()

uint8_t EC_API_SLV_notificationResponse ( uint16_t  idn_p,
uint16_t  channel_p,
uint16_t  dataState_p 
)

Respond to the notification request from the master.

Parameters
[in]idn_pServo identification number.
[in]channel_pchannel parameter.
[in]dataState_pstate description.
Returns
ErrorCode Mailbox error code.
Example
#include <theHeader.h>
// required variables
uint32_t retVal = 0;
void* pvVariable = NULL;
// the Call
retVal = EC_API_SLV_notificationResponse(uint16_t idn, uint16_t channel, uint16_t dataState);
See also
EC_API_SLV_SoE_cbRegisterNotificationReqHandler
EC_API_SLV_notificationResponse
uint8_t EC_API_SLV_notificationResponse(uint16_t idn_p, uint16_t channel_p, uint16_t dataState_p)
Respond to the notification request from the master.
Definition: ecSlvApi_SoEStub.c:208