EtherCAT Slave
1.08.00
◆
EC_API_SLV_PDO_disable()
uint32_t EC_API_SLV_PDO_disable
(
EC_API_SLV_SHandle_t
*
pEcSlaveApi_p
,
EC_API_SLV_SPdo_t
*
pPdo_p
)
Disable PDO assignment to the syncManager.
Parameters
[in]
pEcSlaveApi_p
pointer to API instance.
[in]
pPdo_p
pointer to PDO.
Returns
uint32_t Returns the API error code.
Example
#include <ecSlvApi.h>
// required variables
EC_API_SLV_SHandle_t
* ecSlaveApi;
void
* pvVariable = NULL;
EC_API_SLV_SPdo_t
*ptPdo;
// the Call
retVal =
EC_API_SLV_PDO_disable
(ecSlaveApi, ptPdo);
See also
EC_API_SLV_PDO_enable
EC_API_SLV_SHandle_t
struct EC_API_SLV_SHandle EC_API_SLV_SHandle_t
EC_API_SLV_SHandle_t describes the EtherCAT Slave API.
Definition:
ecSlvApi.h:139
EC_API_SLV_SPdo_t
struct EC_API_SLV_SPdo EC_API_SLV_SPdo_t
TPdo is used to describe the RxPDOs and TxPDOs.
Definition:
ecSlvApi.h:130
EC_API_SLV_PDO_disable
uint32_t EC_API_SLV_PDO_disable(EC_API_SLV_SHandle_t *pEcSlaveApi_p, EC_API_SLV_SPdo_t *pPdo_p)
Disable PDO assignment to the syncManager.
Definition:
ecSlvApi_ProcDataStub.c:1353
PDO Configuration
generated by
1.8.17