EtherCAT Slave  1.08.00

◆ EC_API_SLV_CoE_getObjectEntryCount()

uint32_t EC_API_SLV_CoE_getObjectEntryCount ( EC_API_SLV_SHandle_t pEcSlaveApi_p,
EC_API_SLV_SCoE_Object_t pObject_p,
uint8_t *  pCount_p 
)

This function returns the number of entries of a object.

Returns the number of entries of an object

Parameters
[in]pEcSlaveApi_pThe pointer to the EtherCAT API instance.
[in]pObject_pPointer to the object instance.
[out]pCount_pNumber of entries of the object.
Returns
uint32_t Returns the API error code.
Example
#include <ecSlvApi.h>
// required variables
uint8_t count = 0;
i32uErr_l = EC_API_SLV_CoE_getObjectEntryCount(ecSlaveApi, ptObject, &count);
See also
EC_API_SLV_CoE_getObject EC_API_SLV_CoE_getObjectData EC_API_SLV_CoE_setObjectEntryData
EC_API_SLV_CoE_getObjectEntryCount
uint32_t EC_API_SLV_CoE_getObjectEntryCount(EC_API_SLV_SHandle_t *pEcSlaveApi_p, EC_API_SLV_SCoE_Object_t *pObject_p, uint8_t *pCount_p)
This function returns the number of entries of a object.
Definition: ecSlvApi_CoEStub.c:233