EtherCAT Slave
1.08.00
◆
EC_API_SLV_setState()
uint32_t EC_API_SLV_setState
(
EC_API_SLV_SHandle_t
*
pEcSlaveApi_p
,
EC_API_SLV_EEsmState_t
state_p
)
This is the function to request a EtherCAT state.
Parameters
[in]
pEcSlaveApi_p
Slave API Handle
[in]
state_p
State to set.
Returns
EC_API_EError_t Returns the API error code.
Example
#include <ecSlvApi.h>
EC_API_SLV_setState
(ecSlaveApi, state_p);
EC_API_SLV_setState
uint32_t EC_API_SLV_setState(EC_API_SLV_SHandle_t *pEcSlaveApi_p, EC_API_SLV_EEsmState_t state_p)
This is the function to request a EtherCAT state.
Definition:
ecSlvApiStub.c:1012
Basic Functions
generated by
1.8.17