EtherCAT Slave
1.08.00
◆
EC_API_SLV_getVersionStr()
uint32_t EC_API_SLV_getVersionStr
(
uint32_t
bufLen_p
,
char *
pBuffer_p
,
uint32_t *
pUsedLen_p
)
Get version string.
Parameters
[in]
bufLen_p
Size of provided buffer.
[out]
pBuffer_p
String buffer with version
[out]
pUsedLen_p
Amount of buffer used
Returns
uint32_t errorcode
Example
#include <ecSlvApi.h>
// required variables
uint32_t retVal = 0;
uint32_t used = 0;
char
Version[50] = {0};
// the Call
retVal =
EC_API_SLV_getVersionStr
(
sizeof
(Version), Version, &used);
See also
EC_API_SLV_getVersion
EC_API_SLV_getVersionId
EC_API_SLV_getVersionStr
uint32_t EC_API_SLV_getVersionStr(uint32_t bufLen_p, char *pBuffer_p, uint32_t *pUsedLen_p)
Get version string.
Definition:
ecSlvApiStub.c:180
Basic Functions
generated by
1.8.17