LRE Interface Statistics.
uint32_t RED_STATISTICS::cntTxA |
< Number of frames
uint32_t RED_STATISTICS::cntTxB |
uint32_t RED_STATISTICS::cntTxC |
uint32_t RED_STATISTICS::cntErrWrongLanA |
uint32_t RED_STATISTICS::cntErrWrongLanB |
uint32_t RED_STATISTICS::cntErrWrongLanC |
uint32_t RED_STATISTICS::cntRxA |
uint32_t RED_STATISTICS::cntRxB |
uint32_t RED_STATISTICS::cntRxC |
uint32_t RED_STATISTICS::cntErrorsA |
uint32_t RED_STATISTICS::cntErrorsB |
uint32_t RED_STATISTICS::cntErrorsC |
uint32_t RED_STATISTICS::cntNodes |
Number of entries in the node table
uint32_t RED_STATISTICS::cntProxyNodes |
Number of entries in the proxy table Number of entries in the duplicate detection mechanism
uint32_t RED_STATISTICS::cntUniqueA |
uint32_t RED_STATISTICS::cntUniqueB |
uint32_t RED_STATISTICS::cntUniqueC |
uint32_t RED_STATISTICS::cntDuplicateA |
uint32_t RED_STATISTICS::cntDuplicateB |
uint32_t RED_STATISTICS::cntDuplicateC |
uint32_t RED_STATISTICS::cntMultiA |
uint32_t RED_STATISTICS::cntMultiB |
uint32_t RED_STATISTICS::cntMultiC |
uint32_t RED_STATISTICS::cntOwnRxA |
uint32_t RED_STATISTICS::cntOwnRxB |
uint32_t RED_STATISTICS::cntLookupErrA |
uint32_t RED_STATISTICS::cntLookupErrB |
uint32_t RED_STATISTICS::hostCntRx |
uint32_t RED_STATISTICS::tx_bc_frames |
Numeber of frame retreive by the host
uint32_t RED_STATISTICS::TX_MC_FRAMES |
uint32_t RED_STATISTICS::TX_UC_FRAMES |
uint32_t RED_STATISTICS::TX_BYTE_CNT |
uint32_t RED_STATISTICS::RX_BC_FRAMES |
uint32_t RED_STATISTICS::RX_MC_FRAMES |
uint32_t RED_STATISTICS::RX_UC_FRAMES |
uint32_t RED_STATISTICS::TXB_BC_FRAMES |
uint32_t RED_STATISTICS::TXB_MC_FRAMES |
uint32_t RED_STATISTICS::TXB_UC_FRAMES |
uint32_t RED_STATISTICS::TXB_BYTE_CNT |
uint32_t RED_STATISTICS::RXB_BC_FRAMES |
uint32_t RED_STATISTICS::RXB_MC_FRAMES |
uint32_t RED_STATISTICS::RXB_UC_FRAMES |
uint32_t RED_STATISTICS::NODE_TABLE_INSERTION_ERROR |
uint32_t RED_STATISTICS::RXA_OVERFLOW |
uint32_t RED_STATISTICS::RXB_OVERFLOW |
uint32_t RED_STATISTICS::RXA_FWD_OVERFLOW |
uint32_t RED_STATISTICS::RXB_FWD_OVERFLOW |
uint32_t RED_STATISTICS::RXA_FAILACQU_QUEUE |
uint32_t RED_STATISTICS::RXB_FAILACQU_QUEUE |
uint32_t RED_STATISTICS::RXA_FWD_FAILACQU_QUEUE |
uint32_t RED_STATISTICS::RXB_FWD_FAILACQU_QUEUE |
uint32_t RED_STATISTICS::DEBUG_1 |
uint32_t RED_STATISTICS::DEBUG_2 |
uint32_t RED_STATISTICS::DEBUG_3 |
uint32_t RED_STATISTICS::DEBUG_4 |