AM64x MCU+ SDK  08.03.00

Introduction

This module contains APIs to program and use the PKA.

Files

file  pka.h
 This file contains the prototype of PKA driver APIs.
 

Data Structures

struct  PKA_RSAPubkey
 RSA public key. All values are in biginteger format (size followed by word value array, least significant word first) More...
 
struct  PKA_RSAPrivkey
 RSA private key. All values are in biginteger format (size followed by word value array, least significant word first) More...
 
struct  PKA_ECPoint
 EC Point, also the public key. More...
 
struct  PKA_ECPrimeCurveP
 EC prime curve parameters. More...
 
struct  PKA_ECDSASig
 ECDSA signature. More...
 
struct  PKA_Attrs
 PKA attributes. More...
 
struct  PKA_Config
 PKA driver context. More...
 

Functions

PKA_Handle PKA_open (uint32_t index)
 Function to Open PKA instance, enable PKA engine, Initialize clocks and Load PKA Fw. More...
 
int32_t PKA_close (PKA_Handle handle)
 Function to close a PKA module specified by the PKA handle. More...
 
int32_t PKA_RSAPrivate (PKA_Handle handle, const uint32_t m[PKA_BIGINT_MAX], const struct PKA_RSAPrivkey *k, uint32_t result[PKA_BIGINT_MAX])
 This Function performs Decryption or Signing operations. More...
 
int32_t PKA_RSAPublic (PKA_Handle handle, const uint32_t m[PKA_BIGINT_MAX], const struct PKA_RSAPubkey *k, uint32_t result[PKA_BIGINT_MAX])
 This Function performs Encryption or Verification operations. More...
 
int32_t PKA_ECDSASign (PKA_Handle handle, const struct PKA_ECPrimeCurveP *cp, const uint32_t priv[PKA_EC_BIGINT_MAX], const uint32_t k[PKA_EC_BIGINT_MAX], const uint32_t h[PKA_EC_BIGINT_MAX], struct PKA_ECDSASig *sig)
 ECDSA sign primitive function. More...
 
int32_t PKA_ECDSAVerify (PKA_Handle handle, const struct PKA_ECPrimeCurveP *cp, const struct PKA_ECPoint *pub, const struct PKA_ECDSASig *sig, const uint32_t h[PKA_EC_BIGINT_MAX])
 ECDSA verify primitive function. More...
 

Typedefs

typedef void * PKA_Handle
 Handle to the PKA driver. More...
 

Macros

#define PKA_BIGINT_MAX   (130U)
 
#define PKA_EC_BIGINT_MAX   (18U)
 
#define PKA_EC_PARAM_MAXLEN   (68U)
 
#define PKA_BIGINT_LEN(bytelen)   (((bytelen) / 4U) + 1U)
 
#define PKA_RSA_KEY_E_MAXLEN   (8U)
 
#define PKA_RSA_KEY_N_MAXLEN   (520U)
 
#define PKA_RSA_KEY_PQ_MAXLEN   ((PKA_RSA_KEY_N_MAXLEN / 2U) + 4U)
 
#define PKA_RSA_SIG_MAXLEN   PKA_RSA_KEY_N_MAXLEN
 

Macro Definition Documentation

◆ PKA_BIGINT_MAX

#define PKA_BIGINT_MAX   (130U)

Max size of bigint in words - for RSA

◆ PKA_EC_BIGINT_MAX

#define PKA_EC_BIGINT_MAX   (18U)

Max size of bigint in words - for ECDSA

◆ PKA_EC_PARAM_MAXLEN

#define PKA_EC_PARAM_MAXLEN   (68U)

Maximum length of a big integer used in EC crypto in bytes, enough to accommodate 521-bit prime curves

◆ PKA_BIGINT_LEN

#define PKA_BIGINT_LEN (   bytelen)    (((bytelen) / 4U) + 1U)

Length of a biginteger array in words, the +1 is for the size

◆ PKA_RSA_KEY_E_MAXLEN

#define PKA_RSA_KEY_E_MAXLEN   (8U)

◆ PKA_RSA_KEY_N_MAXLEN

#define PKA_RSA_KEY_N_MAXLEN   (520U)

◆ PKA_RSA_KEY_PQ_MAXLEN

#define PKA_RSA_KEY_PQ_MAXLEN   ((PKA_RSA_KEY_N_MAXLEN / 2U) + 4U)

◆ PKA_RSA_SIG_MAXLEN

#define PKA_RSA_SIG_MAXLEN   PKA_RSA_KEY_N_MAXLEN

Typedef Documentation

◆ PKA_Handle

typedef void* PKA_Handle

Handle to the PKA driver.

Function Documentation

◆ PKA_open()

PKA_Handle PKA_open ( uint32_t  index)

Function to Open PKA instance, enable PKA engine, Initialize clocks and Load PKA Fw.

Returns
A PKA_Handle on success or a NULL on an error or if it has been opened already

◆ PKA_close()

int32_t PKA_close ( PKA_Handle  handle)

Function to close a PKA module specified by the PKA handle.

Parameters
handlePKA_Handle returned from PKA_open()

◆ PKA_RSAPrivate()

int32_t PKA_RSAPrivate ( PKA_Handle  handle,
const uint32_t  m[PKA_BIGINT_MAX],
const struct PKA_RSAPrivkey k,
uint32_t  result[PKA_BIGINT_MAX] 
)

This Function performs Decryption or Signing operations.

Parameters
handlePKA_Handle returned from PKA_open()
mm value in bigint format.
kRSA private key
resultResult of the operation in bigint format. caller must allocate memory size of (2 * sizeof(p)) for the result.
Returns
SystemP_SUCCESS if requested operation completed. SystemP_FAILURE if requested operation not completed.

◆ PKA_RSAPublic()

int32_t PKA_RSAPublic ( PKA_Handle  handle,
const uint32_t  m[PKA_BIGINT_MAX],
const struct PKA_RSAPubkey k,
uint32_t  result[PKA_BIGINT_MAX] 
)

This Function performs Encryption or Verification operations.

Parameters
handlePKA_Handle returned from PKA_open()
mm value in bigint format.
kRSA public key
resultResult of the operation in bigint format. caller must allocate the same memory as s and n for this array.
Returns
SystemP_SUCCESS if requested operation completed. SystemP_FAILURE if requested operation not completed.

◆ PKA_ECDSASign()

int32_t PKA_ECDSASign ( PKA_Handle  handle,
const struct PKA_ECPrimeCurveP cp,
const uint32_t  priv[PKA_EC_BIGINT_MAX],
const uint32_t  k[PKA_EC_BIGINT_MAX],
const uint32_t  h[PKA_EC_BIGINT_MAX],
struct PKA_ECDSASig sig 
)

ECDSA sign primitive function.

Parameters
handlePKA_Handle returned from PKA_open()
cpEC curve parameters
privEC private key
kRandom number for each signing
hHash value of message to sign in bigint format
sigECDSA Signature - 'r' and 's' values
Returns
SystemP_SUCCESS if requested operation completed. SystemP_FAILURE if requested operation not completed.

◆ PKA_ECDSAVerify()

int32_t PKA_ECDSAVerify ( PKA_Handle  handle,
const struct PKA_ECPrimeCurveP cp,
const struct PKA_ECPoint pub,
const struct PKA_ECDSASig sig,
const uint32_t  h[PKA_EC_BIGINT_MAX] 
)

ECDSA verify primitive function.

Parameters
handlePKA_Handle returned from PKA_open()
cpEC curve parameters
pubEC Public key
sigECDSA Signature - 'r' & 's' value in bigint format
hHash value of message to verify in bigint format
Returns
SystemP_SUCCESS if requested operation completed. SystemP_FAILURE if requested operation not completed.

Variable Documentation

◆ gPkaConfig

PKA_Config gPkaConfig[]
extern

Externally defined driver configuration array.

◆ gPkaConfigNum

uint32_t gPkaConfigNum
extern

Externally defined driver configuration Num.