AM64x MCU+ SDK  08.03.00

Introduction

The DMSC firmware Firewall Management system manages SoC Firewall resources. Each firewall in the system is assigned an owner. Ownership is assigned using Host ID. Only a owner of a firewall can:

Files

file  sciclient_firewall.h
 This file contains the definition of all the message IDs, message formats to be able to interact with the System Controller firmware for firewall management.
 

Functions

int32_t Sciclient_firewallChangeOwnerInfo (const struct tisci_msg_fwl_change_owner_info_req *req, struct tisci_msg_fwl_change_owner_info_resp *resp, uint32_t timeout)
 Request for configuring the firewall permissions. More...
 
int32_t Sciclient_firewallSetRegion (const struct tisci_msg_fwl_set_firewall_region_req *req, struct tisci_msg_fwl_set_firewall_region_resp *resp, uint32_t timeout)
 Request for configuring the firewall permissions. More...
 
int32_t Sciclient_firewallGetRegion (const struct tisci_msg_fwl_get_firewall_region_req *req, struct tisci_msg_fwl_get_firewall_region_resp *resp, uint32_t timeout)
 Request for getting the firewall permissions. More...
 

Function Documentation

◆ Sciclient_firewallChangeOwnerInfo()

int32_t Sciclient_firewallChangeOwnerInfo ( const struct tisci_msg_fwl_change_owner_info_req req,
struct tisci_msg_fwl_change_owner_info_resp resp,
uint32_t  timeout 
)

Request for configuring the firewall permissions.


Message: TISCI_MSG_CHANGE_FWL_OWNER
Request: tisci_msg_fwl_change_owner_info_req
Response: tisci_msg_fwl_change_owner_info_resp

Parameters
reqPointer to firewall change owner payload
respPointer to firewall change owner response payload
timeoutGives a sense of how long to wait for the operation. Refer SystemP_Timeout.
Returns
SystemP_SUCCESS on success, else failure

◆ Sciclient_firewallSetRegion()

int32_t Sciclient_firewallSetRegion ( const struct tisci_msg_fwl_set_firewall_region_req req,
struct tisci_msg_fwl_set_firewall_region_resp resp,
uint32_t  timeout 
)

Request for configuring the firewall permissions.


Message: TISCI_MSG_SET_FWL_REGION
Request: tisci_msg_fwl_set_firewall_region_req
Response: tisci_msg_fwl_set_firewall_region_resp

Parameters
reqPointer to firewall region set payload
respPointer to firewall region set response payload
timeoutGives a sense of how long to wait for the operation. Refer SystemP_Timeout.
Returns
SystemP_SUCCESS on success, else failure

◆ Sciclient_firewallGetRegion()

int32_t Sciclient_firewallGetRegion ( const struct tisci_msg_fwl_get_firewall_region_req req,
struct tisci_msg_fwl_get_firewall_region_resp resp,
uint32_t  timeout 
)

Request for getting the firewall permissions.


Message: TISCI_MSG_GET_FWL_REGION
Request: tisci_msg_fwl_get_firewall_region_req
Response: tisci_msg_fwl_get_firewall_region_resp

Parameters
reqPointer to firewall region get payload
respPointer to firewall region get response payload
timeoutGives a sense of how long to wait for the operation. Refer SystemP_Timeout.
Returns
SystemP_SUCCESS on success, else failure