AM64x MCU+ SDK  08.03.00

Introduction

VSC8514 QSGMII Ethernet PHY.

Data Structures

struct  Vsc8514_Cfg
 VSC8514 PHY configuration parameters. More...
 

Functions

void Vsc8514_initCfg (Vsc8514_Cfg *cfg)
 Initialize VSC8514 PHY specific config params. More...
 

Macros

#define VSC8514_LED_NUM   (4U)
 Number of LEDs available in the PHY. More...
 

Macro Definition Documentation

◆ VSC8514_LED_NUM

#define VSC8514_LED_NUM   (4U)

Number of LEDs available in the PHY.

Function Documentation

◆ Vsc8514_initCfg()

void Vsc8514_initCfg ( Vsc8514_Cfg cfg)

Initialize VSC8514 PHY specific config params.

Initializes the VSC8514 PHY specific configuration parameters.

Parameters
cfgVSC8514 PHY config structure pointer