AM64x MCU+ SDK  08.03.00

Introduction

TI DP83869 RGMII Ethernet PHY.

Data Structures

struct  Dp83869_Cfg
 DP83869 PHY configuration parameters. More...
 

Functions

void Dp83869_initCfg (Dp83869_Cfg *cfg)
 Initialize DP83869 PHY specific config params. More...
 

Enumerations

enum  Dp83869_Gpio0Mode {
  DP83869_GPIO0_RXERR = 0x0U, DP83869_GPIO0_1588TXSFD = 0x1U, DP83869_GPIO0_1588RXSFD = 0x2U, DP83869_GPIO0_WOL = 0x3U,
  DP83869_GPIO0_ENERGYDET = 0x4U, DP83869_GPIO0_LED3 = 0x6U, DP83869_GPIO0_PRBSERR = 0x7U, DP83869_GPIO0_CONSTANT0 = 0x8U,
  DP83869_GPIO0_CONSTANT1 = 0x9U
}
 GPIO_0 mux modes. More...
 
enum  Dp83869_Gpio1Mode {
  DP83869_GPIO1_COL = 0x0U, DP83869_GPIO1_1588TXSFD = 0x1U, DP83869_GPIO1_1588RXSFD = 0x2U, DP83869_GPIO1_WOL = 0x3U,
  DP83869_GPIO1_ENERGYDET = 0x4U, DP83869_GPIO1_LED3 = 0x6U, DP83869_GPIO1_PRBSERR = 0x7U, DP83869_GPIO1_CONSTANT0 = 0x8U,
  DP83869_GPIO1_CONSTANT1 = 0x9U
}
 GPIO_1 mux modes. More...
 
enum  Dp83869_LedMode {
  DP83869_LED_LINKED = 0x0U, DP83869_LED_RXTXACT = 0x1U, DP83869_LED_TXACT = 0x2U, DP83869_LED_RXACT = 0x3U,
  DP83869_LED_COLLDET = 0x4U, DP83869_LED_LINKED_1000BT = 0x5U, DP83869_LED_LINKED_100BTX = 0x6U, DP83869_LED_LINKED_10BT = 0x7U,
  DP83869_LED_LINKED_10100BT = 0x8U, DP83869_LED_LINKED_1001000BT = 0x9U, DP83869_LED_FULLDUPLEX = 0xAU, DP83869_LED_LINKED_BLINKACT = 0xBU,
  DP83869_LED_RXTXERR = 0xDU, DP83869_LED_RXERR = 0xEU
}
 LED modes (sources). More...
 

Macros

#define DP83869_LED_NUM   (4U)
 Number of LEDs available in the PHY. More...
 

Macro Definition Documentation

◆ DP83869_LED_NUM

#define DP83869_LED_NUM   (4U)

Number of LEDs available in the PHY.

Enumeration Type Documentation

◆ Dp83869_Gpio0Mode

GPIO_0 mux modes.

Enumerator
DP83869_GPIO0_RXERR 

RX_ER

DP83869_GPIO0_1588TXSFD 

1588 TX SFD

DP83869_GPIO0_1588RXSFD 

1588 RX SFD

DP83869_GPIO0_WOL 

WOL

DP83869_GPIO0_ENERGYDET 

Energy Detect (1000Base-T and 100Base-TX only)

DP83869_GPIO0_LED3 

LED_3

DP83869_GPIO0_PRBSERR 

PRBS Errors / Loss of Sync

DP83869_GPIO0_CONSTANT0 

Constant 0

DP83869_GPIO0_CONSTANT1 

Constant 1

◆ Dp83869_Gpio1Mode

GPIO_1 mux modes.

Enumerator
DP83869_GPIO1_COL 

COL

DP83869_GPIO1_1588TXSFD 

1588 TX SFD

DP83869_GPIO1_1588RXSFD 

1588 RX SFD

DP83869_GPIO1_WOL 

WOL

DP83869_GPIO1_ENERGYDET 

Energy Detect (1000Base-T and 100Base-TX only)

DP83869_GPIO1_LED3 

LED_3

DP83869_GPIO1_PRBSERR 

PRBS Errors / Loss of Sync

DP83869_GPIO1_CONSTANT0 

Constant 0

DP83869_GPIO1_CONSTANT1 

Constant 1

◆ Dp83869_LedMode

LED modes (sources).

Enumerator
DP83869_LED_LINKED 

Link established

DP83869_LED_RXTXACT 

Receive or transmit activity

DP83869_LED_TXACT 

Transmit activity

DP83869_LED_RXACT 

Receive activity

DP83869_LED_COLLDET 

Collision detected

DP83869_LED_LINKED_1000BT 

1000BT link established

DP83869_LED_LINKED_100BTX 

100 BTX link established

DP83869_LED_LINKED_10BT 

10BT link established

DP83869_LED_LINKED_10100BT 

10/100BT link established

DP83869_LED_LINKED_1001000BT 

100/1000BT link established

DP83869_LED_FULLDUPLEX 

Full duplex

DP83869_LED_LINKED_BLINKACT 

Link established, blink for transmit or receive activity

DP83869_LED_RXTXERR 

Receive error or transmit error

DP83869_LED_RXERR 

Receive error

Function Documentation

◆ Dp83869_initCfg()

void Dp83869_initCfg ( Dp83869_Cfg cfg)

Initialize DP83869 PHY specific config params.

Initializes the DP83869 PHY specific configuration parameters.

Parameters
cfgDP83869 PHY config structure pointer