AM64x MCU+ SDK  08.03.00

Introduction

CPSW peripheral supports CPSW_2G, CPSW_5G and CPSW_9G found in SoCs of the Jacinto 7 family.

Features:

Compile-time configuration:

Data Structures

struct  Cpsw_InterVlanRouteIngressPktMatchCfg
 InterVLAN route ingress packet match criteria configuration. More...
 
struct  Cpsw_InterVlanEgressPortCfg
 InterVLAN egress port configuration. More...
 
struct  Cpsw_SetInterVlanRouteUniEgressInArgs
 Input args for CPSW_PER_IOCTL_SET_INTERVLAN_ROUTE_UNI_EGRESS command. More...
 
struct  Cpsw_SetInterVlanRouteUniEgressOutArgs
 Output args for CPSW_PER_IOCTL_SET_INTERVLAN_ROUTE_UNI_EGRESS command. More...
 
struct  Cpsw_ClearInterVlanRouteUniEgressInArgs
 Input args for CPSW_PER_IOCTL_CLEAR_INTERVLAN_ROUTE_UNI_EGRESS command. More...
 
struct  Cpsw_SetInterVlanRouteMultiEgressInArgs
 Input args for CPSW_PER_IOCTL_SET_INTERVLAN_ROUTE_MULTI_EGRESS command. More...
 
struct  Cpsw_SetInterVlanRouteMultiEgressOutArgs
 Output args for CPSW_PER_IOCTL_SET_INTERVLAN_ROUTE_MULTI_EGRESS command. More...
 
struct  Cpsw_ClearInterVlanRouteMultiEgressInArgs
 Input args for CPSW_PER_IOCTL_CLEAR_INTERVLAN_ROUTE_MULTI_EGRESS command. More...
 
struct  Cpsw_SetTxShortIpgCfgInArgs
 Input args for CPSW_PER_IOCTL_SET_SHORT_IPG_CFG. More...
 
struct  Cpsw_TxShortIpgCfg
 Short IPG configuration for CPSW IP. More...
 
struct  Cpsw_VlanCfg
 CPSW-level VLAN configuration. More...
 
struct  Cpsw_MdioLinkStateChangeInfo
 PHY link status change event information. More...
 
struct  Cpsw_Cfg
 CPSW configuration. More...
 

Typedefs

typedef void(* Cpsw_MdioLinkStateChangeCb) (Cpsw_MdioLinkStateChangeInfo *info, void *appArg)
 CPSW PHY link state change callback function. More...
 
typedef void(* Cpsw_PortLinkStatusChangeCb) (Enet_MacPort macPort, bool isLinkUp, void *appArg)
 CPSW port link status change callback function. More...
 

Enumerations

enum  Cpsw_Ioctl {
  CPSW_PER_IOCTL_SET_INTERVLAN_ROUTE_UNI_EGRESS = CPSW_PER_PUBLIC_IOCTL(0U), CPSW_PER_IOCTL_CLEAR_INTERVLAN_ROUTE_UNI_EGRESS = CPSW_PER_PUBLIC_IOCTL(1U), CPSW_PER_IOCTL_SET_INTERVLAN_ROUTE_MULTI_EGRESS = CPSW_PER_PUBLIC_IOCTL(2U), CPSW_PER_IOCTL_CLEAR_INTERVLAN_ROUTE_MULTI_EGRESS = CPSW_PER_PUBLIC_IOCTL(3U),
  CPSW_PER_IOCTL_SET_SHORT_IPG_CFG = CPSW_PER_PUBLIC_IOCTL(4U), CPSW_PER_IOCTL_GET_SHORT_IPG_CFG = CPSW_PER_PUBLIC_IOCTL(5U)
}
 CPSW peripheral IOCTL commands. More...
 

Macros

#define CPSW_PER_PUBLIC_IOCTL(x)
 Helper macro to create CPSW IOCTL commands. More...
 
#define CPSW_MAC_PORT_NUM   (8U)
 
#define CPSW_INTR_STATS_PEND0   (1U)
 CPSW statistics interrupt id. More...
 
#define CPSW_INTR_MDIO_PEND   (2U)
 CPSW MDIO interrupt id. More...
 
#define CPSW_INTR_EVNT_PEND   (3U)
 CPSW event pending interrupt (CPTS) id. More...
 

CPSW InterVLAN ingress packet match types.

Ingress packet match criteria for interVLAN routing. Each packet match criteria is represented by a bit. To enable multiple match criteria create bitmask ORing required ingress packet match criteria defines

#define CPSW_INTERVLAN_INGRESSPKT_MATCH_PORT   (CPSW_ALE_POLICER_MATCH_PORT)
 Enable classifier match with PORT number. More...
 
#define CPSW_INTERVLAN_INGRESSPKT_MATCH_MACSRC   (CPSW_ALE_POLICER_MATCH_MACSRC)
 Enable classifier match with MAC source address entry. More...
 
#define CPSW_INTERVLAN_INGRESSPKT_MATCH_MACDST   (CPSW_ALE_POLICER_MATCH_MACDST)
 Enable classifier match with MAC destination address entry. More...
 
#define CPSW_INTERVLAN_INGRESSPKT_MATCH_ETHERTYPE   (CPSW_ALE_POLICER_MATCH_ETHERTYPE)
 Enable classifier match with MAC destination address entry. More...
 
#define CPSW_INTERVLAN_INGRESSPKT_MATCH_IPSRC   (CPSW_ALE_POLICER_MATCH_IPSRC)
 Enable classifier match with IPv4/IPv6 source address. More...
 
#define CPSW_INTERVLAN_INGRESSPKT_MATCH_IPDST   (CPSW_ALE_POLICER_MATCH_IPDST)
 Enable classifier match with IPv4/IPv6 destination address. More...
 

Macro Definition Documentation

◆ CPSW_PER_PUBLIC_IOCTL

#define CPSW_PER_PUBLIC_IOCTL (   x)
Value:
ENET_IOCTL_PER_BASE | \
ENET_IOCTL_PER_CPSW | \
ENET_IOCTL_MIN(x))

Helper macro to create CPSW IOCTL commands.

◆ CPSW_MAC_PORT_NUM

#define CPSW_MAC_PORT_NUM   (8U)

Maximum number of MAC ports supported by this driver.

◆ CPSW_INTERVLAN_INGRESSPKT_MATCH_PORT

#define CPSW_INTERVLAN_INGRESSPKT_MATCH_PORT   (CPSW_ALE_POLICER_MATCH_PORT)

Enable classifier match with PORT number.

◆ CPSW_INTERVLAN_INGRESSPKT_MATCH_MACSRC

#define CPSW_INTERVLAN_INGRESSPKT_MATCH_MACSRC   (CPSW_ALE_POLICER_MATCH_MACSRC)

Enable classifier match with MAC source address entry.

◆ CPSW_INTERVLAN_INGRESSPKT_MATCH_MACDST

#define CPSW_INTERVLAN_INGRESSPKT_MATCH_MACDST   (CPSW_ALE_POLICER_MATCH_MACDST)

Enable classifier match with MAC destination address entry.

◆ CPSW_INTERVLAN_INGRESSPKT_MATCH_ETHERTYPE

#define CPSW_INTERVLAN_INGRESSPKT_MATCH_ETHERTYPE   (CPSW_ALE_POLICER_MATCH_ETHERTYPE)

Enable classifier match with MAC destination address entry.

◆ CPSW_INTERVLAN_INGRESSPKT_MATCH_IPSRC

#define CPSW_INTERVLAN_INGRESSPKT_MATCH_IPSRC   (CPSW_ALE_POLICER_MATCH_IPSRC)

Enable classifier match with IPv4/IPv6 source address.

◆ CPSW_INTERVLAN_INGRESSPKT_MATCH_IPDST

#define CPSW_INTERVLAN_INGRESSPKT_MATCH_IPDST   (CPSW_ALE_POLICER_MATCH_IPDST)

Enable classifier match with IPv4/IPv6 destination address.

◆ CPSW_INTR_STATS_PEND0

#define CPSW_INTR_STATS_PEND0   (1U)

CPSW statistics interrupt id.

◆ CPSW_INTR_MDIO_PEND

#define CPSW_INTR_MDIO_PEND   (2U)

CPSW MDIO interrupt id.

◆ CPSW_INTR_EVNT_PEND

#define CPSW_INTR_EVNT_PEND   (3U)

CPSW event pending interrupt (CPTS) id.

Typedef Documentation

◆ Cpsw_MdioLinkStateChangeCb

typedef void(* Cpsw_MdioLinkStateChangeCb) (Cpsw_MdioLinkStateChangeInfo *info, void *appArg)

CPSW PHY link state change callback function.

Callback for PHY link state change interrupt (MDIO_LINKINT). This callback is invoked from interrupt context.

◆ Cpsw_PortLinkStatusChangeCb

typedef void(* Cpsw_PortLinkStatusChangeCb) (Enet_MacPort macPort, bool isLinkUp, void *appArg)

CPSW port link status change callback function.

Callback for port link state change event. This callback is invoked when port link is fully functional (PHY linked, ALE ports enabled, etc) or when port link is fully shutdown (ALE ports disabled).

Enumeration Type Documentation

◆ Cpsw_Ioctl

enum Cpsw_Ioctl

CPSW peripheral IOCTL commands.

Enumerator
CPSW_PER_IOCTL_SET_INTERVLAN_ROUTE_UNI_EGRESS 

Setup interVLAN route for a single egress port.

IOCTL parameters:

CPSW_PER_IOCTL_CLEAR_INTERVLAN_ROUTE_UNI_EGRESS 

Setup interVLAN route for a single egress port.

IOCTL parameters:

CPSW_PER_IOCTL_SET_INTERVLAN_ROUTE_MULTI_EGRESS 

Setup interVLAN route for a multiple egress port.

IOCTL parameters:

CPSW_PER_IOCTL_CLEAR_INTERVLAN_ROUTE_MULTI_EGRESS 

Clear interVLAN route for a multiple egress port route.

IOCTL parameters:

CPSW_PER_IOCTL_SET_SHORT_IPG_CFG 

Configure short inter-packet gap (IPG) for specific MAC ports.

IOCTL parameters:

CPSW_PER_IOCTL_GET_SHORT_IPG_CFG 

Get the current short inter-packet gap (IPG) configuration for all open MAC ports.

IOCTL parameters:

ENET_IOCTL_TYPE_PUBLIC
@ ENET_IOCTL_TYPE_PUBLIC
Definition: enet_ioctl.h:167