#include <PN_API_PDEV.h>
Data Fields | |
uint16_t | deviceDescriptionLength |
uint8_t * | pDeviceDescription |
uint16_t | orderIdLength |
uint8_t * | pOrderId |
uint16_t | serialNumberLength |
uint8_t * | pSerialNumber |
uint16_t | hwRevisionLength |
uint8_t * | pHwRevision |
uint8_t | swRevisionPrefix |
uint16_t | swRevisionFunctionalEnhancementLength |
uint8_t * | pSwRevisionFunctionalEnhancement |
uint16_t | swRevisionBugFixLength |
uint8_t * | pSwRevisionBugFix |
uint16_t | swRevisionInternalChangeLength |
uint8_t * | pSwRevisionInternalChange |