#include <PN_API_ETH.h>
Data Fields | |
uint8_t | numberOfPeers |
PN_API_ETH_SPeerCheck_t | aPeers [PN_API_ETH_MAX_PEERS_PER_PORT] |
bool | checkLineDelay |
uint8_t | lineDelayFormat |
uint32_t | lineDelay |
bool | checkMauType |
uint16_t | mauType |
bool | checkLinkState |
uint8_t | linkStateLink |
uint8_t | linkStatePort |
bool | checkSyncDiff |
uint8_t | syncMaster |
uint8_t | cableDelay |
bool | checkMauTypeMode |
uint8_t | mauTypeMode |