uint32_t PN_API_IM_removeImCarrier | ( | PN_API_IM_SCarrierAddress_t * | pAddress_p | ) |
Remove an I&M carrier from stack.
With this function application removes an I&M carrier from the stack. Concerned submodule has no attached I&M data anymore.
[in] | pAddress_p | Address of I&M carrier, which is being removed. |
PN_API_IM_eOK | Function successful. |
PN_API_IM_eERR_REMOVE_IM_INVALID_POINTER | Invalid parameters (NULL pointers). |
PN_API_IM_eERR_REMOVE_IM_CARRIER_NOT_EXIST | Specified I&M carrier does not exist. |