EtherNet/IP™ Adapter  1.04.06
User Reference Manual

◆ EI_API_ADP_setTimeSyncSupported()

uint32_t EI_API_ADP_setTimeSyncSupported ( T pAdp_p)

Enable Time Sync Object support.

Enable Time Sync support. This function should only be called for applications that require EtherNet/IP Time Sync functionality.

Parameters
[in]pAdp_pPointer to the adapter.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
// Enable Time Sync
errCode = EI_API_ADP_setTimeSyncSupported(pEI_API_ADP);
EI_API_ADP_setTimeSyncSupported
ETHIP_API uint32_t EI_API_ADP_setTimeSyncSupported(T *pAdp_p)
Enable Time Sync Object support.
Definition: EI_API_ADP_main.c:1812
EI_API_ADP_new
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:235