EtherNet/IP™ Adapter  1.04.06
User Reference Manual

◆ EI_API_ADP_getEncapInactTimeout()

uint32_t EI_API_ADP_getEncapInactTimeout ( T pAdp_p,
uint16_t *  pEncapInactTimeout_p 
)

Get the current adapter encapsulation inactivity timeout (Instance Attribute ID: 13).

Function that returns the adapter encapsulation inactivity timeout in the return value.

Parameters
[in]pAdp_pPointer to the adapter.
[out]pEncapInactTimeout_pPoint of type uint16_t to the adapter encapsulation inactivity timeout value (seconds).
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
uint16_t encapInactTimeout;
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
errCode = EI_API_ADP_getEncapInactTimeout(pEI_API_ADP, &encapInactTimeout);
See also
EI_API_ADP_setEncapInactTimeout EI_API_ADP_EError_t
EI_API_ADP_getEncapInactTimeout
ETHIP_API uint32_t EI_API_ADP_getEncapInactTimeout(T *pAdp_p, uint16_t *pEncapInactTimeout_p)
Get the current adapter encapsulation inactivity timeout (Instance Attribute ID: 13).
Definition: EI_API_ADP_main.c:5145
EI_API_ADP_new
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:235