EtherNet/IP™ Adapter  1.04.06
User Reference Manual

◆ EI_API_ADP_setEnipAcdState()

uint32_t EI_API_ADP_setEnipAcdState ( T pAdp_p,
uint8_t  enipAcdState_p 
)

Set the current adapter Ethernet IP address conflict detection state (Instance Attribute ID: 11).

Function that sets the adapter IP address conflict detection state.

Parameters
[in]pAdp_pPointer to the adapter.
[in]enipAcdState_pIP address conflict detection state.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
// Reset IP address conflict detection state
errCode = EI_API_ADP_setEnipAcdState(pEI_API_ADP, 0x00);
See also
EI_API_ADP_getEnipAcdState EI_API_ADP_EError_t
EI_API_ADP_setEnipAcdState
ETHIP_API uint32_t EI_API_ADP_setEnipAcdState(T *pAdp_p, uint8_t enipAcdState_p)
Set the current adapter Ethernet IP address conflict detection state (Instance Attribute ID: 11).
Definition: EI_API_ADP_main.c:4577
EI_API_ADP_new
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:235