EtherNet/IP™ Adapter  1.04.06
User Reference Manual

◆ EI_API_ADP_getRevision()

uint32_t EI_API_ADP_getRevision ( T pAdp_p,
EI_API_ADP_SRevision_t pRevision_p 
)

Get the adapter Revision (Instance Attribute ID: 4).

Function that returns the revision of the adapter selected by parameter pAdp_p. The revision attribute is divided into major and minor revision number.

Parameters
[in]pAdp_pPointer to the adapter.
[out]pRevision_pPointer to an adapter revision structure.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
errCode = EI_API_ADP_getRevision(pEI_API_ADP, &revision);
See also
EI_API_ADP_setRevision EI_API_ADP_SRevision_t EI_API_ADP_EError_t
EI_API_ADP_getRevision
ETHIP_API uint32_t EI_API_ADP_getRevision(T *pAdp_p, EI_API_ADP_SRevision_t *pRevision_p)
Get the adapter Revision (Instance Attribute ID: 4).
Definition: EI_API_ADP_main.c:1333
EI_API_ADP_SRevision
Definition: EI_API_ADP.h:132
EI_API_ADP_new
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:235