EtherNet/IP™ Adapter
1.04.06
User Reference Manual
◆
EI_API_ADP_startFirmware()
void EI_API_ADP_startFirmware
(
void
)
Enable PRU firmware.
Remarks
Must be called after
EI_API_ADP_loadMac
.
Example
#include <api/EI_API.h>
EIP_SLoadParameter
tParam;
uint32_t errCode;
memset (&tParam, 0,
sizeof
(
EIP_SLoadParameter
));
memmove (tParam.
ai8uMacAddr
, EI_APP_getMacAddr(), 6);
errCode =
EI_API_ADP_loadMac
(pEI_API_ADP, EI_API_ADP_PRUICCSS_INSTANCE_TWO);
EI_API_ADP_startFirmware
();
See also
EI_API_ADP_loadMac
EIP_SLoadParameter
Definition:
EI_API_ADP.h:167
EI_API_ADP_loadMac
ETHIP_API uint32_t EI_API_ADP_loadMac(EIP_SLoadParameter *ptPara_p, uint8_t pruInstance)
Load and initialize EthernetIP firmware in PRU.
Definition:
EI_API_ADP_main.c:104
EI_API_ADP_startFirmware
ETHIP_API void EI_API_ADP_startFirmware(void)
Enable PRU firmware.
Definition:
EI_API_ADP_main.c:180
EIP_SLoadParameter::ai8uMacAddr
uint8_t ai8uMacAddr[EIP_MAC_ADDR_LEN]
Definition:
EI_API_ADP.h:168
Basic Functions
generated by
1.8.18