void EC_API_SLV_cbRegisterStartOutputHandler | ( | EC_API_SLV_SHandle_t * | pEcSlaveApi_p, |
void * | pContext_p, | ||
EC_API_SLV_CBStartOutputHandler_t | cbFunc_p | ||
) |
This is the function to register a function which starts the output handler.
The function is called in the state transition from SAFEOP to OP when all general settings were checked to start the output handler. This function informs the application about the state transition, the application can refuse the state transition when returning an AL Status error code. The return code NOERROR_INWORK can be used, if the application cannot confirm the state transition immediately, in that case this function will be called cyclically until a value unequal NOERROR_INWORK is returned
[in] | pEcSlaveApi_p | The pointer to the EtherCAT API instance. |
[in] | pContext_p | startOuputHandler call context |
[in] | cbFunc_p | Function pointer to the Start Output Handler |