EtherCAT Slave  1.06.01

◆ EC_API_SLV_writeDoubleWordEscRegister()

void EC_API_SLV_writeDoubleWordEscRegister ( EC_API_SLV_SHandle_t pEcSlaveApi_p,
uint16_t  escAddress_p,
uint32_t  value_p 
)
Parameters
[in]pEcSlaveApi_pThe pointer to the EtherCAT API instance.
[in]escAddress_pThe ESC Address
[in]value_pNew value
Example
#include <ecSlvApi.h>
// required variables
uint32_t alEscCtrlStatus = 8;
// the Call
EC_API_SLV_writeDoubleWordEscRegister(ecSlaveApi, 0x120, alEscCtrlStatus);
See also
theReference
EC_API_SLV_writeDoubleWordEscRegister
void EC_API_SLV_writeDoubleWordEscRegister(EC_API_SLV_SHandle_t *pEcSlaveApi_p, uint16_t escAddress_p, uint32_t value_p)
Definition: ecSlvApiStub.c:1320