AM64x MCU+ SDK  08.02.00

Detailed Description

OSPI Parameters.

OSPI Parameters are used to with the OSPI_open() call. Default values for these parameters are set using OSPI_Params_init().

If NULL is passed for the parameters, OSPI_open() uses default parameters.

See also
OSPI_Params_init()

Data Fields

int32_t ospiDmaChIndex
 

Field Documentation

◆ ospiDmaChIndex

int32_t OSPI_Params::ospiDmaChIndex