uint8_t OSPI_GenericXspiDevDefines::XSPI_NOR_CMD_RSTEN |
uint8_t OSPI_GenericXspiDevDefines::XSPI_NOR_CMD_RSTMEM |
uint8_t OSPI_GenericXspiDevDefines::XSPI_NOR_CMD_WREN |
uint8_t OSPI_GenericXspiDevDefines::XSPI_NOR_CMD_WRREG |
uint8_t OSPI_GenericXspiDevDefines::XSPI_NOR_CMD_BULK_ERASE |
uint8_t OSPI_GenericXspiDevDefines::XSPI_NOR_CMD_SECTOR_ERASE_3B |
uint8_t OSPI_GenericXspiDevDefines::XSPI_NOR_CMD_SECTOR_ERASE_4B |
uint8_t OSPI_GenericXspiDevDefines::XSPI_NOR_CMD_BLOCK_ERASE_3B |
uint8_t OSPI_GenericXspiDevDefines::XSPI_NOR_CMD_BLOCK_ERASE_4B |
uint8_t OSPI_GenericXspiDevDefines::XSPI_NOR_CMD_PAGE_PROG_3B |
uint8_t OSPI_GenericXspiDevDefines::XSPI_NOR_CMD_PAGE_PROG_4B |
uint8_t OSPI_GenericXspiDevDefines::XSPI_NOR_CMD_RDSR |
uint8_t OSPI_GenericXspiDevDefines::XSPI_NOR_CMD_RDREG |
uint8_t OSPI_GenericXspiDevDefines::XSPI_NOR_CMD_RDID |
uint8_t OSPI_GenericXspiDevDefines::XSPI_NOR_CMD_READ |
uint8_t OSPI_GenericXspiDevDefines::XSPI_NOR_CMD_888_SDR_READ |
uint8_t OSPI_GenericXspiDevDefines::XSPI_NOR_CMD_888_DDR_READ |
uint8_t OSPI_GenericXspiDevDefines::XSPI_NOR_CMD_444_SDR_READ |
uint8_t OSPI_GenericXspiDevDefines::XSPI_NOR_CMD_444_DDR_READ |
uint8_t OSPI_GenericXspiDevDefines::XSPI_NOR_CMD_114_READ |
uint32_t OSPI_GenericXspiDevDefines::XSPI_NOR_SR_WIP |
uint32_t OSPI_GenericXspiDevDefines::XSPI_NOR_SR_WEL |
uint8_t OSPI_GenericXspiDevDefines::XSPI_NOR_RDID_NUM_BYTES |
uint8_t OSPI_GenericXspiDevDefines::XSPI_NOR_MANF_ID |
uint16_t OSPI_GenericXspiDevDefines::XSPI_NOR_DEVICE_ID |
uint16_t OSPI_GenericXspiDevDefines::XSPI_NOR_114_READ_MODE_CLKS |
uint16_t OSPI_GenericXspiDevDefines::XSPI_NOR_114_READ_DUMMY_CYCLES |
uint16_t OSPI_GenericXspiDevDefines::XSPI_NOR_114_READ_DUMMY_CYCLES_LC |
uint16_t OSPI_GenericXspiDevDefines::XSPI_NOR_444_READ_MODE_CLKS |
uint16_t OSPI_GenericXspiDevDefines::XSPI_NOR_444_READ_DUMMY_CYCLES |
uint16_t OSPI_GenericXspiDevDefines::XSPI_NOR_444_READ_DUMMY_CYCLES_LC |
uint16_t OSPI_GenericXspiDevDefines::XSPI_NOR_QUAD_CMD_READ_DUMMY_CYCLES |
uint16_t OSPI_GenericXspiDevDefines::XSPI_NOR_OCTAL_READ_DUMMY_CYCLE |
uint16_t OSPI_GenericXspiDevDefines::XSPI_NOR_OCTAL_READ_DUMMY_CYCLE_LC |
uint16_t OSPI_GenericXspiDevDefines::XSPI_NOR_OCTAL_DDR_RDSR_DUMMY_CYCLE |
uint16_t OSPI_GenericXspiDevDefines::XSPI_NOR_OCTAL_DDR_RDSR_ADDR_BYTES |
uint16_t OSPI_GenericXspiDevDefines::XSPI_NOR_OCTAL_DDR_RDREG_ADDR_BYTES |
uint16_t OSPI_GenericXspiDevDefines::XSPI_NOR_OCTAL_DDR_WRREG_ADDR_BYTES |
uint16_t OSPI_GenericXspiDevDefines::XSPI_NOR_OCTAL_DDR_RDVREG_DUMMY_CYCLE |
uint16_t OSPI_GenericXspiDevDefines::XSPI_NOR_OCTAL_DDR_RDNVREG_DUMMY_CYCLE |
uint16_t OSPI_GenericXspiDevDefines::XSPI_NOR_OCTAL_RDSFDP_DUMMY_CYCLE |
uint8_t OSPI_GenericXspiDevDefines::XSPI_NOR_OCTAL_RDSFDP_ADDR_TYPE |
uint32_t OSPI_GenericXspiDevDefines::XSPI_NOR_WRR_WRITE_TIMEOUT |
uint32_t OSPI_GenericXspiDevDefines::XSPI_NOR_BULK_ERASE_TIMEOUT |
uint32_t OSPI_GenericXspiDevDefines::XSPI_NOR_PAGE_PROG_TIMEOUT |
uint32_t OSPI_GenericXspiDevDefines::XSPI_NOR_VREG_OFFSET |
uint32_t OSPI_GenericXspiDevDefines::XSPI_NOR_NVREG_OFFSET |
uint32_t OSPI_GenericXspiDevDefines::XSPI_NOR_QUAD_MODE_CFG_ADDR |
uint32_t OSPI_GenericXspiDevDefines::XSPI_NOR_QUAD_MODE_CFG_BIT_LOCATION |
uint32_t OSPI_GenericXspiDevDefines::XSPI_NOR_DDR_OCTAL_MODE_CFG_ADDR |
uint32_t OSPI_GenericXspiDevDefines::XSPI_NOR_DDR_OCTAL_MODE_CFG_BIT_LOCATION |
uint32_t OSPI_GenericXspiDevDefines::XSPI_NOR_DUMMY_CYCLE_CFG_ADDR |
uint64_t OSPI_GenericXspiDevDefines::XSPI_NOR_FLASH_SIZE |
uint16_t OSPI_GenericXspiDevDefines::XSPI_NOR_PAGE_SIZE |
uint32_t OSPI_GenericXspiDevDefines::XSPI_NOR_BLOCK_SIZE |
uint32_t OSPI_GenericXspiDevDefines::XSPI_NOR_SECTOR_SIZE |
uint8_t OSPI_GenericXspiDevDefines::addrByteSupport |
uint8_t OSPI_GenericXspiDevDefines::dtrSupport |
uint8_t OSPI_GenericXspiDevDefines::qeType |
uint8_t OSPI_GenericXspiDevDefines::seq444Enable[5] |
uint8_t OSPI_GenericXspiDevDefines::seq444Disable[4] |
uint8_t OSPI_GenericXspiDevDefines::oeType |
uint8_t OSPI_GenericXspiDevDefines::cmdExtType |
uint8_t OSPI_GenericXspiDevDefines::byteOrder |
uint8_t OSPI_GenericXspiDevDefines::supportedEraseTypes[2] |