AM64x MCU+ SDK  08.02.00

Detailed Description

Flash device attributes, these are filled by SysCfg based on the flash device that is selected.

Data Fields

uint32_t deviceId
 
uint32_t manufacturerId
 
uint32_t driverInstance
 
uint32_t flashSize
 
uint32_t blockCount
 
uint32_t blockSize
 
uint32_t pageCount
 
uint32_t pageSize
 
uint32_t sectorCount
 
uint32_t sectorSize
 

Field Documentation

◆ deviceId

uint32_t Flash_Attrs::deviceId

Flash device ID as read form the flash device, this will be filled when Flash_open() is called

◆ manufacturerId

uint32_t Flash_Attrs::manufacturerId

Flash manufacturer ID as read form the flash device, this will be filled when Flash_open() is called

◆ driverInstance

uint32_t Flash_Attrs::driverInstance

Underlying OSPI peripheral driver instance that is used by the flash driver, e.g OSPI driver

◆ flashSize

uint32_t Flash_Attrs::flashSize

Flash size, in bytes

◆ blockCount

uint32_t Flash_Attrs::blockCount

Number of blocks in the flash the flash

◆ blockSize

uint32_t Flash_Attrs::blockSize

Size of each block, in bytes

◆ pageCount

uint32_t Flash_Attrs::pageCount

Number of pages per block

◆ pageSize

uint32_t Flash_Attrs::pageSize

Size of each page, in bytes

◆ sectorCount

uint32_t Flash_Attrs::sectorCount

Number of sectors in the flash, if flash supports sectors

◆ sectorSize

uint32_t Flash_Attrs::sectorSize

Size of each flash sector, in bytes