PHY State-Machine time-out values.
Data Fields | |
uint32_t | findingStateTicks |
FINDING state timeout (in ticks) More... | |
uint32_t | resetWaitStateTicks |
RESET_WAIT state timeout (in ticks) More... | |
uint32_t | resetWaitStateResidenceTicks |
RESET_WAIT state residence time (in ticks) More... | |
uint32_t | nwayStartStateTicks |
NWAY_START state timeout (in ticks) More... | |
uint32_t | nwayWaitStateTicks |
NWAY_WAIT state timeout (in ticks) More... | |
uint32_t | linkWaitStateTicks |
LINK_WAIT state timeout (in ticks) More... | |
uint32_t | mdixTicks |
Timeout if MDIX is enabled (in ticks) More... | |
uint32_t EnetPhy_FsmTimeoutCfg::findingStateTicks |
FINDING state timeout (in ticks)
uint32_t EnetPhy_FsmTimeoutCfg::resetWaitStateTicks |
RESET_WAIT state timeout (in ticks)
uint32_t EnetPhy_FsmTimeoutCfg::resetWaitStateResidenceTicks |
RESET_WAIT state residence time (in ticks)
uint32_t EnetPhy_FsmTimeoutCfg::nwayStartStateTicks |
NWAY_START state timeout (in ticks)
uint32_t EnetPhy_FsmTimeoutCfg::nwayWaitStateTicks |
NWAY_WAIT state timeout (in ticks)
uint32_t EnetPhy_FsmTimeoutCfg::linkWaitStateTicks |
LINK_WAIT state timeout (in ticks)
uint32_t EnetPhy_FsmTimeoutCfg::mdixTicks |
Timeout if MDIX is enabled (in ticks)