CPSW 2G host port statistics.
Statistics values reported by the CPSW hardware for the host port.
uint64_t CpswStats_HostPort_2g::rxGoodFrames |
Total number of good frames received
uint64_t CpswStats_HostPort_2g::rxBcastFrames |
Total number of good multicast frames received
uint64_t CpswStats_HostPort_2g::rxMcastFrames |
Total number of good multicast frames received
uint64_t CpswStats_HostPort_2g::reserved4 |
Reserved
uint64_t CpswStats_HostPort_2g::rxCrcErrors |
Total number of CRC error frames received
uint64_t CpswStats_HostPort_2g::reserved6 |
Reserved
uint64_t CpswStats_HostPort_2g::rxOversizedFrames |
Total number of oversized frames received
uint64_t CpswStats_HostPort_2g::reserved8 |
Reserved
uint64_t CpswStats_HostPort_2g::rxUndersizedFrames |
Total number of undersized frames received
uint64_t CpswStats_HostPort_2g::rxFragments |
Total number of fragmented frames received
uint64_t CpswStats_HostPort_2g::aleDrop |
Total number of frames dropped by the ALE
uint64_t CpswStats_HostPort_2g::aleOverrunDrop |
Total number of overrun frames dropped by the ALE
uint64_t CpswStats_HostPort_2g::rxOctets |
Total number of received bytes in good frames
uint64_t CpswStats_HostPort_2g::txGoodFrames |
Total number of good frames transmitted
uint64_t CpswStats_HostPort_2g::txBcastFrames |
Total number of good broadcast frames transmitted
uint64_t CpswStats_HostPort_2g::txMcastFrames |
Total number of good multicast frames transmitted
uint64_t CpswStats_HostPort_2g::reserved17to25[9U] |
Reserved
uint64_t CpswStats_HostPort_2g::txOctets |
Total number of bytes in all good frames transmitted
uint64_t CpswStats_HostPort_2g::octetsFrames64 |
Total number of 64-byte frames received and transmitted
uint64_t CpswStats_HostPort_2g::octetsFrames65to127 |
Total number of frames of size 65 to 127 bytes received and transmitted
uint64_t CpswStats_HostPort_2g::octetsFrames128to255 |
Total number of frames of size 128 to 255 bytes received and transmitted
uint64_t CpswStats_HostPort_2g::octetsFrames256to511 |
Total number of frames of size 256 to 511 bytes received and transmitted
uint64_t CpswStats_HostPort_2g::octetsFrames512to1023 |
Total number of frames of size 512 to 1023 bytes received and transmitted
uint64_t CpswStats_HostPort_2g::octetsFrames1024 |
Total number of frames of size 1024 or greater transmitted
uint64_t CpswStats_HostPort_2g::netOctets |
Total number of bytes received and transmitted
uint64_t CpswStats_HostPort_2g::rxBottomOfFifoDrop |
Receive bottom of FIFO drop
uint64_t CpswStats_HostPort_2g::portMaskDrop |
Total number of dropped frames received due to portmask
uint64_t CpswStats_HostPort_2g::rxTopOfFifoDrop |
Receive top of FIFO drop
uint64_t CpswStats_HostPort_2g::aleRateLimitDrop |
Total number of frames dropped due to ALE rate limiting
uint64_t CpswStats_HostPort_2g::aleVidIngressDrop |
Total number of dropped frames due to ALE VID ingress
uint64_t CpswStats_HostPort_2g::aleDAEqSADrop |
Total number of dropped frames due to DA = SA
uint64_t CpswStats_HostPort_2g::aleBlockDrop |
Total number of dropped frames due to ALE block mode
uint64_t CpswStats_HostPort_2g::aleSecureDrop |
Total number of dropped frames due to ALE secure mode
uint64_t CpswStats_HostPort_2g::aleAuthDrop |
Total number of dropped frames due to ALE authentication
uint64_t CpswStats_HostPort_2g::aleUnknownUcast |
ALE receive unknown unicast
uint64_t CpswStats_HostPort_2g::aleUnknownUcastBcnt |
ALE receive unknown unicast bytecount
uint64_t CpswStats_HostPort_2g::aleUnknownMcast |
ALE receive unknown multicast
uint64_t CpswStats_HostPort_2g::aleUnknownMcastBcnt |
ALE receive unknown multicast bytecount
uint64_t CpswStats_HostPort_2g::aleUnknownBcast |
ALE receive unknown broadcast
uint64_t CpswStats_HostPort_2g::aleUnknownBcastBcnt |
ALE receive unknown broadcast bytecount
uint64_t CpswStats_HostPort_2g::alePolicyMatch |
ALE policer matched
uint64_t CpswStats_HostPort_2g::alePolicyMatchRed |
ALE policer matched and condition red
uint64_t CpswStats_HostPort_2g::alePolicyMatchYellow |
ALE policer matched and condition yellow
uint64_t CpswStats_HostPort_2g::reserved52to95[44U] |
Reserved
uint64_t CpswStats_HostPort_2g::txMemProtectError |
Transmit memory protect CRC error
uint64_t CpswStats_HostPort_2g::reserved97to128[32U] |
Reserved